Interesting, I am experiencing the same issue with the reTerminal as the original poster.
Attached is the log of the errors, and a repeat of the issues above.
No joy … still a blank screen.
pi@mana-controller:~ $ sudo apt install git -y
git clone --depth 1 https://github.com/Seeed-Studio/seeed-linux-dtoverlays
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
git is already the newest version (1:2.30.2-1+deb11u2).
The following package was automatically installed and is no longer required:
raspinfo
Use 'sudo apt autoremove' to remove it.
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.
Cloning into 'seeed-linux-dtoverlays'...
remote: Enumerating objects: 859, done.
remote: Counting objects: 100% (859/859), done.
remote: Compressing objects: 100% (705/705), done.
remote: Total 859 (delta 157), reused 694 (delta 124), pack-reused 0
Receiving objects: 100% (859/859), 2.15 MiB | 1001.00 KiB/s, done.
Resolving deltas: 100% (157/157), done.
pi@mana-controller:~ $ cd seeed-linux-dtoverlays
pi@mana-controller:~/seeed-linux-dtoverlays $ cat /boot/config.txt
# For more options and information see
# http://rpf.io/configtxt
# Some settings may impact device functionality. See link above for details
# uncomment if you get no picture on HDMI for a default "safe" mode
#hdmi_safe=1
# uncomment the following to adjust overscan. Use positive numbers if console
# goes off screen, and negative if there is too much border
#overscan_left=16
#overscan_right=16
#overscan_top=16
#overscan_bottom=16
# uncomment to force a console size. By default it will be display's size minus
# overscan.
#framebuffer_width=1280
#framebuffer_height=720
# uncomment if hdmi display is not detected and composite is being output
#hdmi_force_hotplug=1
# uncomment to force a specific HDMI mode (this will force VGA)
#hdmi_group=1
#hdmi_mode=1
# uncomment to force a HDMI mode rather than DVI. This can make audio work in
# DMT (computer monitor) modes
#hdmi_drive=2
# uncomment to increase signal to HDMI, if you have interference, blanking, or
# no display
#config_hdmi_boost=4
# uncomment for composite PAL
#sdtv_mode=2
#uncomment to overclock the arm. 700 MHz is the default.
#arm_freq=800
# Uncomment some or all of these to enable the optional hardware interfaces
dtparam=i2c_arm=on
#dtparam=i2s=on
#dtparam=spi=on
# Uncomment this to enable infrared communication.
#dtoverlay=gpio-ir,gpio_pin=17
#dtoverlay=gpio-ir-tx,gpio_pin=18
# Additional overlays and parameters are documented /boot/overlays/README
# Enable audio (loads snd_bcm2835)
dtparam=audio=on
# Automatically load overlays for detected cameras
camera_auto_detect=1
# Automatically load overlays for detected DSI displays
display_auto_detect=1
# Enable DRM VC4 V3D driver
dtoverlay=vc4-kms-v3d
max_framebuffers=2
# Disable compensation for displays with overscan
disable_overscan=1
[cm4]
# Enable host mode on the 2711 built-in XHCI USB controller.
# This line should be removed if the legacy DWC2 controller is required
# (e.g. for USB device mode) or if USB support is not required.
otg_mode=1
[all]
[pi4]
# Run as fast as firmware / board allows
arm_boost=1
[all]
enable_uart=1
dtoverlay=dwc2,dr_mode=host
dtparam=ant2
disable_splash=1
ignore_lcd=1
dtoverlay=vc4-kms-v3d-pi4
dtoverlay=i2c3,pins_4_5
gpio=13=pu
dtoverlay=reTerminal,tp_rotate=1
dtoverlay=reTerminal-bridge
pi@mana-controller:~/seeed-linux-dtoverlays $ cat /proc/cpuinfo
processor : 0
BogoMIPS : 108.00
Features : fp asimd evtstrm crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd08
CPU revision : 3
processor : 1
BogoMIPS : 108.00
Features : fp asimd evtstrm crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd08
CPU revision : 3
processor : 2
BogoMIPS : 108.00
Features : fp asimd evtstrm crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd08
CPU revision : 3
processor : 3
BogoMIPS : 108.00
Features : fp asimd evtstrm crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd08
CPU revision : 3
Hardware : BCM2835
Revision : c03141
Serial : 10000000d3510466
Model : Raspberry Pi Compute Module 4 Rev 1.1
pi@mana-controller:~/seeed-linux-dtoverlays $ uname -na
Linux mana-controller 6.1.21-v8+ #1642 SMP PREEMPT Mon Apr 3 17:24:16 BST 2023 aarch64 GNU/Linux
pi@mana-controller:~/seeed-linux-dtoverlays $ sudo ./scripts/reTerminal.sh
### Install required tool packages
Hit:1 http://raspbian.raspberrypi.org/raspbian bullseye InRelease
Hit:2 http://archive.raspberrypi.org/debian bullseye InRelease
Reading package lists... Done
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
dkms is already the newest version (2.8.4-3).
The following package was automatically installed and is no longer required:
raspinfo
Use 'sudo apt autoremove' to remove it.
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.
### Will compile with the latest kernel...
### Uninstall previous dkms module
------------------------------
Deleting module version: 0.1
completely from the DKMS tree.
------------------------------
Done.
------------------------------
Deleting module version: 0.1
completely from the DKMS tree.
------------------------------
Done.
------------------------------
Deleting module version: 0.1
completely from the DKMS tree.
------------------------------
Done.
------------------------------
Deleting module version: 0.1
completely from the DKMS tree.
------------------------------
Done.
removed '/boot/overlays/reTerminal.dtbo'
### Install required kernel package
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
raspberrypi-kernel is already the newest version (1:1.20230405-1).
raspberrypi-kernel-headers is already the newest version (1:1.20230405-1).
The following package was automatically installed and is no longer required:
raspinfo
Use 'sudo apt autoremove' to remove it.
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.
W: --force-yes is deprecated, use one of the options starting with --allow instead.
KBUILD: /lib/modules/6.1.21-v7l+/build
Creating symlink /var/lib/dkms/mipi_dsi/0.1/source ->
/usr/src/mipi_dsi-0.1
DKMS: add completed.
Kernel preparation unnecessary for this kernel. Skipping...
Building module:
cleaning build area...(bad exit status: 2)
make -j4 KERNELRELEASE=6.1.21-v7l+ all KVERSION=6.1.21-v7l+...(bad exit status: 2)
Error! Bad return status for module build on kernel: 6.1.21-v7l+ (aarch64)
Consult /var/lib/dkms/mipi_dsi/0.1/build/make.log for more information.
Can't compile with this kernel, aborting
Please try to compile with the option --compat-kernel
DKMS make.log for mipi_dsi-0.1 for kernel 6.1.21-v7l+ (aarch64)
Mon 05 Feb 2024 01:21:54 PM PST
make -C /lib/modules/6.1.21-v7l+/build M=/var/lib/dkms/mipi_dsi/0.1/build modules
make[1]: Entering directory '/usr/src/linux-headers-6.1.21-v7l+'
CC [M] /var/lib/dkms/mipi_dsi/0.1/build/mipi_dsi_drv.o
CC [M] /var/lib/dkms/mipi_dsi/0.1/build/touch_panel.o
CC [M] /var/lib/dkms/mipi_dsi/0.1/build/panel-ili9881d.o
In file included from ./include/linux/types.h:6,
from ./include/linux/limits.h:6,
from ./include/linux/kernel.h:16,
from ./include/linux/interrupt.h:6,
from /var/lib/dkms/mipi_dsi/0.1/build/mipi_dsi.h:15,
from /var/lib/dkms/mipi_dsi/0.1/build/panel-ili9881d.c:8:
./include/uapi/linux/types.h:5:10: fatal error: asm/types.h: No such file or directory
5 | #include <asm/types.h>
| ^~~~~~~~~~~~~
In file included from ./include/linux/types.h:6,
from ./include/linux/limits.h:6,
from ./include/linux/kernel.h:16,
from ./include/linux/interrupt.h:6,
from /var/lib/dkms/mipi_dsi/0.1/build/mipi_dsi.h:15,
from /var/lib/dkms/mipi_dsi/0.1/build/mipi_dsi_drv.c:11:
./include/uapi/linux/types.h:5:10: fatal error: asm/types.h: No such file or directory
5 | #include <asm/types.h>
| ^~~~~~~~~~~~~
In file included from ./include/linux/types.h:6,
from ./include/linux/limits.h:6,
from ./include/linux/kernel.h:16,
from ./include/linux/interrupt.h:6,
from /var/lib/dkms/mipi_dsi/0.1/build/mipi_dsi.h:15,
from /var/lib/dkms/mipi_dsi/0.1/build/touch_panel.c:1:
./include/uapi/linux/types.h:5:10: fatal error: asm/types.h: No such file or directory
5 | #include <asm/types.h>
| ^~~~~~~~~~~~~
compilation terminated.
compilation terminated.
compilation terminated.
make[2]: *** [scripts/Makefile.build:250: /var/lib/dkms/mipi_dsi/0.1/build/mipi_dsi_drv.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[2]: *** [scripts/Makefile.build:250: /var/lib/dkms/mipi_dsi/0.1/build/touch_panel.o] Error 1
make[2]: *** [scripts/Makefile.build:250: /var/lib/dkms/mipi_dsi/0.1/build/panel-ili9881d.o] Error 1
make[1]: *** [Makefile:2012: /var/lib/dkms/mipi_dsi/0.1/build] Error 2
make[1]: Leaving directory '/usr/src/linux-headers-6.1.21-v7l+'
make: *** [Makefile:15: all] Error 2