That is a more than odd response tbh.
Circuitpython already has far more drivers than MicroPython and has a large amount of graphics related libraries that are perfect for hardware like the Wio Terminal.
Mass Storage based programming is also far more convenient. I really hope you reconsider that position.
Actually whether this can be supported or not depends on Adafruit’s attitude. They simply need to add a pin map and usb vid/pid in the code to support it. However, this information is completely open source. @timonsku@olivier-boesch
Hi hi, I’m Scott, the lead for CircuitPython. Me and others are paid by Adafruit to work full-time on CircuitPython.
We love to see non-Adafruit boards supported in CircuitPython. (There are already many.) We will always review pull requests for any addition to CircuitPython including non-Adafruit boards. Those of us paid by Adafruit will only provide limited support for non-Adafruit boards though. It is expected that the board manufacturer is the main contact for support.
In this case it means we won’t add the Wio Terminal ourselves but would happily merge a PR for it.
Adafruit provides USB PIDs to hobby boards for use in CircuitPython but expects companies who sell boards to have a USB VID of their own that they can use in CircuitPython.
ArduPy looks neat and I am curious to see what parts people want to integrate back into CircuitPython. As I said before, we’re always happy to review PRs.
Suggest LoRa can be DASH7, SX1262 can be used as a DASH7 device with a specific firmware flashed. I prefer DASH7 to LoRa due to the industry advantages of DASH7.
If possible, there could be an external EEPROM to extend the program, while an AI helper could be integrated. That will be a powerful ML device for IoT.
How about adding 4G/5G support to the Wio so that the device can be used anywhere?
More ideas may occur to me, but I think the features I mentioned above could make this approaching to an advanced IoT terminal for both hobbyists and professionals.
@tannewt
Hi Scott, it is really nice to have you here. We really appreciate what circuit python has done and hopefully we will soon have PR regarding wio terminal for circuit python. Keeping it up.
@ONLYA
You’re absolutely right, ArduPy was designed with the intention that he would be able to use the product in a professional way.
Thanks Scott, this is Eric Pan from Seeed. We appreicate the openess!
Ardupy is taking quite a different approach and serving different purposes more towards industrial tool. We will surely consider circuit python as users are now asking for it. Cheers!
I have a project that needs accurate timer so I would like an accurate RTC with an interrupt such as DS3231 to fit in the enclosure. Needs 3v SDA SCL and IO for the square wave
Other requests:
GPS module for position and timing. Needs serial, power and IO for pps signal.
Small plugs to cover up unused ports.
Could the battery chassis have an alternative deeper back to accommodate a 40 pin breakout and user extension boards?
I noticed a 1 mm misalignment between the Wio Terminal and the battery extension, both vertically and horizontally.
I’ve just read the warning about the Wio Terminal Battery Chassis.
The charge current will up to 1.5A, which may reduce battery life or cause other issues.
We are optimizing the design of the new version (the estimated release date is unavailable yet), and we recommend the new version if you are a beginner.
*Please contact us for tech support or exchange if you meet any problem during the usage of this version.
It would be nice to have the ability to turn off the yellow and red LEDs through code, if that’s not already possible. Unfortunately this battery is not very useful over the long term if you can’t reduce the amount of power for projects that require lower power.
The second version of the battery chassis is great with the built-in power management.
The LoRa chassis will turn the Wio Terminal into a hub, collecting and processing data from node through LoRa, and pushing aggregated summary to the web.
Finally, the I²S chassis will offer an introduction to audio management. Maybe a talkie-walkie?
The battery chassis is super! I have an idea to make it better usable together with wio terminal: If there is an application installed on wio terminal which is not running 24 hours a day, but only sometimes if user wants see something and maybe work with the application for some seconds or minutes, then the battery button on the chassis can be switched off for longer times. But for switching battery power on and off, some tool like a pen is needed to do that. Now my idea: if wio terminal recognizes that battery pack is connected, battery could be switched off and on when wio terminal slide button is switched off or on.