Comparison of Sleep Current for XIAO nRF54L15, nRF52840, and MG24

I compared the sleep current of the newly released nRF54L15 with the nRF52840 and MG24, known for their low power consumption. I hope this proves useful.

Measurements were taken using ppk2 while applying 3.8V to the battery pads on the device’s back. Since sleep current is highly sensitive to temperature, room temperature was maintained as close to 25°C as possible.
For the BSP, I used “Seeed nRF52 Boards 1.1.10” for the nRF52840 and “Silicon Labs 3.0.0” for the MG24, working within the capabilities of the Arduino IDE. The nRF54L15 was worked on in a VsCode + PlatformIO environment. No tricky operations were performed to lower the current values.
Comparison results:

  1. Deep sleep current is sufficiently low at around 2uA, showing no significant difference.
  2. Light sleep(idle) current is significantly worse for MG24 at 60uA.
  3. As an example of operating current, I compared the current during execution of while(mills()-timestamp);. The nRF54L15 shows significantly lower current consumption.

Overall, the nRF54L15 appears to be the most power-efficient device.

Results may vary depending on device-specific tuning. Please share any additional information you have.
The code used for the experiment is attached below.
XIAO_SleepCurrent.zip (6.5 KB)

Hi there,

So I feel like some PLUG is needed here, and so much more to be discovered. If seeed would take full advantage more could be gained.
Also Some of the users having issues may not be aware of the Power domains and turning things on when needed, I’m just starting to Scratch the silicon surface :grin:
Thank you for the efforts and enlightenment :bowing_man:

PLUG :grin:

The nRF54L Series is among the first publicly available low-power wireless SoCs fabricated using 22 nm process technology. This technology offers high transistor density, lower average power consumption, and improved process efficiency, enabling the creation of compact, efficient, and feature-rich chips for advanced applications.

To optimize energy consumption, the nRF54L Series architecture is divided into four power domains that are independently powered, depending on what features are active at any point in time. This architecture enables ultra-low-power operation by allowing domains to be powered independently, allowing large sections of the chip to be turned off when not actively needed.

HTH
GL :slight_smile: PJ :v:

When discussing XIAO’s sleep current, the current consumption of onboard devices other than the MPU must be considered. The most dominant factor is the SBD leakage current, which exhibits significant variation and is temperature-sensitive.

[typ. uA]              nRF54L15   nRF52840      MG24
MPU            I_sleep   0.6       0.4          0.25
SBD            Ir         5       Unknown         5
3.3V Reg       Iq        0.3         1           0.3
LevelShifter   IccA       2          -            -
Measured Value Ioff      1.7       2.4           1.6

Interesting discovery :thinking:
So, with BLE, Zigbee, Matter support out of the box, a stable development and complete environment (including Micropython), the EFR32MG24 is looking to be quite a “favourable” option? (Yes, in Australia and other Commonwealth countries, there is a “u” in “favourable” :smiley: )

The MG24 has excellent sleep current values, comparable to the nRF, but its operating current consumption when the radio is active seems less favorable. I suspect the transmit stage amplifier design is fundamentally different.

‘Comparison of Advertising Current for XIAO nRF54L15, nRF52840, and MG24’

Hi there,

So , “Better” depends on the job. MG24 absolutely has a very nice ‘out-of-the-box’ story for Zigbee/Thread/Matter (and even CircuitPython).
But on raw efficiency, nRF54L15 wins the common cases: ~3.3–3.4 mA RX and ~4.8–5.2 mA @0 dBm TX, with ~0.8 µA System-OFF + RTC. MG24’s own datasheet lists ~4.4 mA RX and ~5.0 mA @0 dBm TX. Also, 54L15 does include 802.15.4, so Thread/Matter aren’t off the table. Pick the part for your constraints—ecosystem speed vs. lifetime on a coin cell. :grin:

Compute & headroom:
nRF54L15 runs a 128 MHz M33 (+ RISC-V coprocessor) with up to 1.5 MB NVM / 256 KB RAM. MG24 tops out at ~78 MHz M33 with up to 1.5 MB / 256 KB. If you need more CPU cycles per joule, 54L15 has the architectural advantage.

MG24 has SKUs with +20 dBm—fantastic for range, but you’ll pay for it (~156 mA at max power). If you don’t need that PA, the comparison should be apples-to-apples at 0 dBm.

So is MG24 “more favourable”?

If your priority is quickest path to Zigbee/Thread/Matter and Python-based prototyping:* sure, MG24 is easier out of the gate for now. :crossed_fingers:

If your priority is battery life for BLE-centric sensors/trackers, plus more CPU per µA: the nRF54L15 is hard to beat right now. :grin: :+1:

I can say though at 4-5 weeks the info is avalanching with updates coming in a timely manner. Giving it time to marinate and propagate you can’t beat the support they offer over the other companies.

GL :slight_smile: PJ :v:

more to come, forsure from the NORDs… :grin:

Thanks for the correction.

I have a few weeks “spare” before my customer’s prototype boards arrive so hopefully “the Nords, Vikings etc” have a suitable solution to these “teething” problems?

Hi there,

really nice informations here!

I have one point I want to throw in here regarding the XIAO nrf54L15. It has an antenna switch (FM8625H) which has to be powered if you want a good HF signal. According to the datasheet, the FM8625H needs about 100µA supply current. Which of course is huge! And somehow ruins the low current requirements of the nRF54L15. So IMHO the nRF54L15 is a very good choice for lowest power applications, but not the XIAO nRF54L15. I really don’t understand why the XIAO has the antenna switch, it would be much better if there were two versions, one with chip antenna and another one with external antenna and no HF switch!

HTH
Hannes

For XIAO MG24: disabling the debug interface greatly reduces current during sleep(), as Matthieu_Charbonnier found out, see ‘Power consumption of XIAO MG24’ thread.

HTH
Hannes

I apologize for not starting a new thread for this, but as a new member evidently, I cannot. Using a XAIO nrf54L15 and the Seeed low power example, I cannot get below 5ma as measured by the PPK2. It doesn’t matter if I power via the Vbus , Vbat or 3.3V pin. Anyone have any idea why I am not coming in at the few ua values everyone else seems to get? I built the example using Nordic SDK version 3.3.2 using the board files supplied in the platform-seedboards tree.

keck9939,

Have you tried the project attached to Post #1?

What I tried was very similar, but not identical. I ran the example in post 1 and am getting 5ma where the comment indicates it should be 1.7ma, 2.3ma where the comment says 3ua and 230ua where the comment says 1.7ua. I’ve ordered a nRF54L15DK board for testing and I’ll order another XIAO nRF54L15 on the assumption that something is wrong with the one I’ve got.

Nothing is connected to the XIAO_nRF54L15 except for the ppk2, right?

The only thing connected is the PPK2. It turns out, if I connect to Vbat at 3.8 volts, as specified in Post 1, I actually get pretty much what the comments say. I was originally connected to 3.3v at 3.3v.

Now, it will be interesting to see if I can get anywhere near that in my actual application, (Matter over Thread temperature sensor).

If the project goes well, please be sure to let us know the results.