For flashing a bootloader yes, you need a UART (there may be options like RS232<->UART converter) and the easiest way is tu buy a USB<->TTL adapter. Cheap like hell. Can do your own as well (e.g. roboforum.ru/forum4/topic10592-15.html#p232256 - sorry, it’s in Russian). If you use a scope you need other convenient tools, so it’s a good investment. You can also consider more complicated tools like BusPirate. Does an awful lot of things but it will take time to learn how to handle it.
Also, there was a piece of software that did *.hex to *.bin convertation. Will try to find it for you - can’t remember what’s the name of it…
Right, search for “usb ttl” on eBay and you can find them for less than 3 $ (with Free Shipping/Buy Now), including cables. Seeed only sells more specialized usb to serial boards as far as I can see.
On Linux you can use:
objcopy -I ihex -O binary file.hex file.bin
Anyway, I guess the problem is not the differently formatted hex files, but that eDesign(?) has added some checksum or “certificate” to make sure only their firmwares can be installed. Effectively shooting themselves in the foot, since their firmware is a joke compared to the independent third-party firmware from Benf.
I just flashed the BenF software on the DSO201 with the the new bootloader.
I took the hex files generated by the IAR Compiler and also changed the file names. (V201_LIB.HEX, V201_APP.HEX) and now it works. DSO201Flash.zip (34.2 KB)
Alf, that has fixed it for me as well. Haven’t checked it all but looks good so far.
Many many thanks to you and everyone who has devoted time to solve this problem.
I won’t be sending my nano back now, now going to learn the ins and outs of benf’s app.
Just a quick question, it comes up as app ver 3.11 how does this differ from the 3.64 app?
Thanks again
I copied the source code here: gitorious.org/dsonano/dso-firmware#more
But this seems to be not the actual version of the BenF SW. If i can get the source for BenF 3.64 i could try the same again.
Hi Alf, have had a look at this 3.11 and it is much much better than the e-design 2.60 but has a few features missing that are in 3.64, if you could work your miracle on the 3.64 app and lib that would be great.
The benf 3.64 is in this forum under “DSO firmware version 3.64” and the file is on the first message, don’t know if this is what you mean you need?
Hello, in this file are only the DFU files and a PDF, no source code. You can convert the DFU files to the hex file with the DFU File Manager but the bootloader can’t handle the generated format. The hex files generated by the IAR workbench seems to work, at least the version that i tested. I will try to get the source code.
Hi Alf, yes I now grasp what you mean, excuse me but I am a hardware engineer so get a bit confused by all this compiling etc
I have had a quick look and it may well be that the last source code available may well be the 3.11 however I will keep hunting and put any info on here, maybe others with this problem can have a search as well to see what can be found?
Alf, looks like you have cracked it. Loaded fine and comes up as 3.64, extra featuresa all seem there, about to sit down and play.
Many thanks again to you and everyone else.
Good job, alf! Glad you got it working, and that my guess about checksums/certification was proven wrong. For your information, BenF’s 3.13 version was the last open-source version, there are only minor changes to what’s in the git tree on gitorious.
I used the IAR Embedded Workbench 6.3 (6.30.7.3447)
Thanks for the info about the BenF Source code, so i will not search for the code any more.
At the moment i am glad that it works.
Yes its interesting why the hex file I posted from a zip Benf 3.1 for IAR5 I got from Google code did not work. Maybe the file name matters or maybe IAR 6 format is different. Anyways I glad Alf skills came in handy.
Alf, greatest thanks. You are a genius! I bow to your expertise and generosity in providing these files in a format/design that is functional with the DSO201 V1 with the new boot loader.
I had a potential nightmare on my hands. I found a .hex that worked online somewhere else…but it was miss labeled and ended up being V1.1 firmware. Not very pretty…
Your two files worked perfectly for me. Up until I came across your post I could not get various .hex to work with new boot loader version.
I now have functional Ben F Firmware; LIB 3.64 APP 3.53. I’m off to go explore its features
Hello everyone,
I came to this forum after buying a nano DSU by a Chinese vendor who seemed seriously, this is the
link diyertool.com/measuring-equi … so201.html
I have discovered that it is equipped with the updater firmeare V3.20A …
reading this tread I was able to load version benf, but I was wondering if in the future, the inability to use
the system bootloader with the program of classic St, might be a problem …
if I contact the seller, I can claim to have been cheated, because the product is not what I bought?