XIAOESP32S3-Sense Does Not Broadcast its Setup SSID

Hi there,

So, OK I see what your looking for, but two things, The heatsinks? you WILL need them, Second is the SD card installed ?, 32Gig class A that bit me hard in this thread which you should have already read. :crossed_fingers: :grin:

Did you try to put your WIFI credentials in, to join your own wifi network SSID, password :crossed_fingers: You may have an older firmware, I’m suspecting that :face_with_hand_over_mouth: try that and see if the serial output changes.

lmk ,
HTH
GL :slight_smile: PJ :v:

you may just need to rebuild it from the examples in arduino, try the latest BSP and Flash it, see if it responds. I use the WPS code works every time, easy piece of code to blend into any wifi scenario, I have demo’s of that and video on here. ( I can press the wps button from the browser window).:+1: