Hi there,
check this link, here… demo the DS18B20 working in the B-roll. so see it there.
Here is the code I used in the demo.
/**************************************************************************
This is an example of the Cheepest OLEDs based on SSD1306 & a DS18B20 Temp sensor.
connected to a grove Expansion Board.
Pick one up today in the adafruit shop!
------> http://www.adafruit.com/category/63_98
This example is for a 128x32 pixel display using I2C to communicate
3 pins are required to interface (two I2C and one reset).
/**************************************************************************/
#include <Arduino.h>
#include <SPI.h>
#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>
#include <OneWire.h>
#include <DallasTemperature.h>
//#include <Fonts/FreeSerif12pt7b.h>
//#include <Fonts/FreeSerif9pt7b.h>
#define ONE_WIRE_BUS D7
OneWire oneWire(ONE_WIRE_BUS);
DallasTemperature DS18B20(&oneWire);
#define SCREEN_WIDTH 128 // OLED display width, in pixels
#define SCREEN_HEIGHT 32 // OLED display height, in pixels
// Define monochrome graphics:
static const unsigned char PROGMEM _error [] = {
0x00, 0x00, 0x00, 0x00, 0x00, 0x3F, 0xFC, 0x00, 0x00, 0xE0, 0x07, 0x00, 0x01, 0x80, 0x01, 0x80,
0x06, 0x00, 0x00, 0x60, 0x0C, 0x00, 0x00, 0x30, 0x08, 0x01, 0x80, 0x10, 0x10, 0x03, 0xC0, 0x08,
0x30, 0x02, 0x40, 0x0C, 0x20, 0x02, 0x40, 0x04, 0x60, 0x02, 0x40, 0x06, 0x40, 0x02, 0x40, 0x02,
0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x02,
0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x02, 0x40, 0x03, 0xC0, 0x02, 0x40, 0x01, 0x80, 0x02,
0x40, 0x00, 0x00, 0x02, 0x60, 0x00, 0x00, 0x06, 0x20, 0x01, 0x80, 0x04, 0x30, 0x03, 0xC0, 0x0C,
0x10, 0x03, 0xC0, 0x08, 0x08, 0x01, 0x80, 0x10, 0x0C, 0x00, 0x00, 0x30, 0x06, 0x00, 0x00, 0x60,
0x01, 0x80, 0x01, 0x80, 0x00, 0xE0, 0x07, 0x00, 0x00, 0x3F, 0xFC, 0x00, 0x00, 0x00, 0x00, 0x00
};
// Define the data holders:
//float t = m_temperature;
float temps, m_temperature;
int class_number = 0;
long timer;
uint16_t error;
char errorMessage[256];
// Declaration for an SSD1306 display connected to I2C (SDA, SCL pins)
#define OLED_RESET -1 // Reset pin # (or -1 if sharing Arduino reset pin)
#define SCREEN_ADDRESS 0x3C ///< See datasheet for Address; 0x3D for 128x64, 0x3C for 128x32
Adafruit_SSD1306 display(SCREEN_WIDTH, SCREEN_HEIGHT, &Wire, OLED_RESET);
#define NUMFLAKES 10 // Number of snowflakes in the animation example
#define LOGO_HEIGHT 12
#define LOGO_WIDTH 12
static const unsigned char PROGMEM logo_bmp[] =
{ 0b00000000, 0b11000000,
0b00000001, 0b11000000,
0b00000001, 0b11000000,
0b00000011, 0b11100000,
0b11110011, 0b11100000,
0b11111110, 0b11111000,
0b01111110, 0b11111111,
0b00110011, 0b10011111,
0b00011111, 0b11111100,
0b00001101, 0b01110000,
0b00011011, 0b10100000,
0b00111111, 0b11100000,
0b00111111, 0b11110000,
0b01111100, 0b11110000,
0b01110000, 0b01110000,
0b00000000, 0b00110000 };
const int buttonPin = 2; // the number of the pushbutton pin
int buttonState = 0; // variable for reading the pushbutton status
uint8_t binterruptCount = 0; // Amount of received interrupts
const int BuzzerPin = 0;
int buzzer = BuzzerPin;
#define LEDR LED_BUILTIN // default
#define LEDG LED_GREEN
#define LEDB LED_BLUE
uint8_t interruptCount = 0; // Amount of received interrupts
uint8_t prevInterruptCount = 0; // Interrupt Counter from last loop
bool first10LoopCompleted = false;
int deviceCount = 0; // variable to store the number of devices connected
DeviceAddress deviceAddress; // variable to store the device address
void setup() {
Wire.begin();
delay(250);
Serial.begin(9600);
delay(2000);
DS18B20.begin();
//while (!Serial) delay(2100); // Code will wait until USB port is plugged in.
pinMode(BuzzerPin, OUTPUT);
buzzer = LOW ; // Buzzer OFF
Serial.println();
Serial.println("Program " __FILE__ " compiled on " __DATE__ " at " __TIME__);
Serial.println();
Serial.println("Processor came out of reset.");
Serial.println();
//pinMode(D7, INPUT); // Ds180
delay (500);
// Locate the devices on the bus:
Serial.println("Locating devices...");
Serial.print("Found ");
deviceCount = DS18B20.getDeviceCount();
Serial.print(deviceCount);
Serial.println(" devices");
Serial.println("Printing addresses...");
for (int i = 0; i < deviceCount; i++) {
Serial.print("Sensor ");
Serial.print(i + 1);
Serial.print(" : ");
DS18B20.getAddress(deviceAddress, i);
printAddress(deviceAddress);
}
// SSD1306_SWITCHCAPVCC = generate display voltage from 3.3V internally
if(!display.begin(SSD1306_SWITCHCAPVCC, 0x3C)) {
Serial.println(F("SSD1306 allocation failed"));
for(;;); // Don't proceed, loop forever
}
display.display();
delay(2000); // Pause for 2 seconds
// Clear the buffer
display.clearDisplay();
// Draw a single pixel in white
display.drawPixel(10, 10, SSD1306_WHITE);
// Show the display buffer on the screen. You MUST call display() after
// drawing commands to make them visible on screen!
display.display();
delay(1000);
//testdrawchar(); // Draw characters of the default font
//testdrawstyles(); // Draw 'stylized' characters
testscrolltext(); // Draw scrolling text
testdrawbitmap(); // Draw a small bitmap image
// Invert and restore display, pausing in-between
display.invertDisplay(true);
delay(500);
display.invertDisplay(false);
delay(500);
//testanimate(logo_bmp, LOGO_WIDTH, LOGO_HEIGHT); // Animate bitmaps
mTemperature();
}
void loop() {
testscrolltext(); // Draw scrolling text
delay (2000);
mTemperature();
delay (3000);
}
void mTemperature(){
// Obtain the temperature measurement generated by the DS18B20 Waterproof Temperature Sensor.
DS18B20.setResolution(10);
DS18B20.requestTemperatures();
float ctemp = DS18B20.getTempCByIndex(0);
m_temperature = DS18B20.getTempFByIndex(0);
Serial.print("\n Temperature: "); Serial.print(m_temperature); Serial.println("°F");
delay(250);
display.clearDisplay(); // Clear display buffer
display.setTextSize(1); // Normal 1:1 pixel scale
display.setTextColor(WHITE); // Draw white text
display.setCursor(0, 0); // Start at top-left corner
display.display();
display.print("TEMP is:\n"); //Flash Test:0123456789
display.setTextSize(3);
display.print(m_temperature);
display.setTextSize(1);
display.print("F");
display.display();
delay(1100);
}
void printAddress(DeviceAddress deviceAddress) {
for (uint8_t i = 0; i < 8; i++) {
Serial.print("0x");
if (deviceAddress[i] < 0x10) {
Serial.print("0");
}
Serial.print(deviceAddress[i], HEX);
if (i < 7) {
Serial.print(", ");
}
}
Serial.println(" done...");
}
void testdrawchar(void) {
display.clearDisplay();
display.setTextSize(1); // Normal 1:1 pixel scale
display.setTextColor(SSD1306_WHITE); // Draw white text
display.setCursor(0, 0); // Start at top-left corner
display.cp437(true); // Use full 256 char 'Code Page 437' font
// Not all the characters will fit on the display. This is normal.
// Library will draw what it can and the rest will be clipped.
for(int16_t i=0; i<128; i++) {
if(i == '\n') display.write(' ');
else display.write(i);
}
display.display();
delay(1000);
}
void err_msg(){
// Show the error message on the SSD1306 screen.
display.clearDisplay();
display.drawBitmap(48, 0, _error, 32, 32, SSD1306_WHITE);
display.setTextSize(1);
display.setTextColor(SSD1306_WHITE);
display.setCursor(0,40);
display.println("Check the serial monitor to see the error!");
display.display();
}
void testdrawstyles(void) {
display.clearDisplay();
display.setTextSize(1); // Normal 1:1 pixel scale
display.setTextColor(SSD1306_WHITE); // Draw white text
display.setCursor(0,0); // Start at top-left corner
display.println(F("Hello, DUDE!! "));
display.setTextColor(SSD1306_BLACK, SSD1306_WHITE); // Draw 'inverse' text
display.println(3.141592);
display.setTextSize(2); // Draw 2X-scale text
display.setTextColor(SSD1306_WHITE);
display.print(F("0x")); display.println(0xDEADBEEF, HEX);
display.display();
delay(500);
}
void testscrolltext(void) {
display.clearDisplay();
display.setTextSize(1); // Draw 2X-scale text
display.setTextColor(SSD1306_WHITE);
display.setCursor(10, 0);
display.print(F("Temp Is\n"));
display.display(); // Show initial text
delay(100);
// Scroll in various directions, pausing in-between:
display.startscrollright(0x00, 0x0F);
delay(2300);
display.stopscroll();
delay(200);
display.startscrollleft(0x00, 0x0F);
delay(2500);
display.stopscroll();
display.setTextColor(SSD1306_BLACK);
display.setCursor(10, 0);
display.print("Temp Is");
display.display(); // Show initial text
delay(300);
display.setTextColor(SSD1306_WHITE);
display.setTextSize(2); // Draw 2X-scale text
display.setCursor(0, 10);
float ctemp = DS18B20.getTempFByIndex(0);
delay(250);
display.print(ctemp);
display.print(" ");
display.setTextSize(1);
display.print("F");
delay(2000);
display.display();
delay(2000);
display.startscrolldiagright(0x00, 0x07);
delay(2000);
display.startscrolldiagleft(0x00, 0x07);
delay(2000);
display.stopscroll();
delay(2000);
}
void testdrawbitmap(void) {
display.clearDisplay();
display.drawBitmap(
(display.width() - LOGO_WIDTH ) / 2,
(display.height() - LOGO_HEIGHT) / 2,
logo_bmp, LOGO_WIDTH, LOGO_HEIGHT, 1);
display.display();
delay(1000);
}
#define XPOS 0 // Indexes into the 'icons' array in function below
#define YPOS 1
#define DELTAY 2
void testanimate(const uint8_t *bitmap, uint8_t w, uint8_t h) {
int8_t f, icons[NUMFLAKES][3];
// Initialize 'snowflake' positions
for(f=0; f< NUMFLAKES; f++) {
icons[f][XPOS] = random(1 - LOGO_WIDTH, display.width());
icons[f][YPOS] = -LOGO_HEIGHT;
icons[f][DELTAY] = random(1, 6);
Serial.print(F("x: "));
Serial.print(icons[f][XPOS], DEC);
Serial.print(F(" y: "));
Serial.print(icons[f][YPOS], DEC);
Serial.print(F(" dy: "));
Serial.println(icons[f][DELTAY], DEC);
}
for(;;) { // Loop forever...
display.clearDisplay(); // Clear the display buffer
// Draw each snowflake:
for(f=0; f< NUMFLAKES; f++) {
display.drawBitmap(icons[f][XPOS], icons[f][YPOS], bitmap, w, h, SSD1306_WHITE);
}
display.display(); // Show the display buffer on the screen
delay(200); // Pause for 1/10 second
// Then update coordinates of each flake...
for(f=0; f< NUMFLAKES; f++) {
icons[f][YPOS] += icons[f][DELTAY];
// If snowflake is off the bottom of the screen...
if (icons[f][YPOS] >= display.height()) {
// Reinitialize to a random position, just off the top
icons[f][XPOS] = random(1 - LOGO_WIDTH, display.width());
icons[f][YPOS] = -LOGO_HEIGHT;
icons[f][DELTAY] = random(1, 6);
}
}
}
}
Hope That Helps
GL , PJ ![]()
here is Compiler output
FQBN: Seeeduino:nrf52:xiaonRF52840Sense
Using board 'xiaonRF52840Sense' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8
Using core 'nRF5' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8
edit----for Brevity----
Zip created at C:\Users\Dude\AppData\Local\Temp\arduino\sketches\CC942BAF52BC74DA90551B61D261992E/Display_DS18B20_SSD1306_DEMO.ino.zip
Multiple libraries were found for "Adafruit_TinyUSB.h"
Used: D:\Arduino_projects\libraries\Adafruit_TinyUSB_Library
Not used: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8\libraries\Adafruit_TinyUSB_Arduino
Using library SPI at version 1.0 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8\libraries\SPI
Using library Wire at version 1.0 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.8\libraries\Wire
Using library Adafruit GFX Library at version 1.11.9 in folder: D:\Arduino_projects\libraries\Adafruit_GFX_Library
Using library Adafruit BusIO at version 1.16.1 in folder: D:\Arduino_projects\libraries\Adafruit_BusIO
Using library Adafruit SSD1306 at version 2.5.10 in folder: D:\Arduino_projects\libraries\Adafruit_SSD1306
Using library OneWire at version 2.3.8 in folder: D:\Arduino_projects\libraries\OneWire
Using library DallasTemperature at version 3.9.0 in folder: D:\Arduino_projects\libraries\DallasTemperature
Using library Adafruit TinyUSB Library at version 3.1.5 in folder: D:\Arduino_projects\libraries\Adafruit_TinyUSB_Library
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\tools\\arm-none-eabi-gcc\\9-2019q4/bin/arm-none-eabi-size" -A "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\CC942BAF52BC74DA90551B61D261992E/Display_DS18B20_SSD1306_DEMO.ino.elf"
Sketch uses 71392 bytes (8%) of program storage space. Maximum is 811008 bytes.
Global variables use 8564 bytes (3%) of dynamic memory, leaving 229004 bytes for local variables. Maximum is 237568 bytes.