XIAO Round Display + ESP32S3

Hi,

I recently got a new GC9A01 display, but I haven’t been able to get it working with an ESP32S3.

I found a really helpful guide by Mark Lucking HERE but even following that, I still couldn’t get it to work. Here’s what I’ve managed so far:

----- Code

#include <TFT_eSPI.h>
#include <SPI.h>
#define USE_TFT_ESPI_LIBRARY
#include “lv_xiao_round_screen.h”

lv_coord_t touchX, touchY;

void setup() {
// put your setup code here, to run once:
Serial.begin(115200);

pinMode(TOUCH_INT, INPUT_PULLUP);
Wire.begin();

// Initialise the screen
tft.init();

tft.setRotation(0);
tft.fillScreen(TFT_BLACK);
}

void loop() {
//put your main code here, to run repeatedly:
if(chsc6x_is_pressed())
{
Serial.println(“The display is touched.”);
chsc6x_get_xy(&touchX, &touchY);
tft.drawCircle(touchX, touchY, 15, TFT_WHITE);
}

delay(500);
}
------ TFT_eSPI User_Setup

#define USER_SETUP_INFO “User_Setup”
#define GC9A01_DRIVER
#define TFT_HEIGHT 240 // GC9A01 240 x 240
#define TFT_CS   PIN_D8  // Chip select control pin D8
#define TFT_DC   PIN_D3  // Data Command control pin
#define TFT_RST  PIN_D4  // Reset pin (could connect to NodeMCU RST, see next line)
// Use an Arduino pin for initial testing as connecting to processor reset
// may not work (pulse too short at power up?)
#define LOAD_GLCD   // Font 1. Original Adafruit 8 pixel font needs ~1820 bytes in FLASH
#define LOAD_FONT2  // Font 2. Small 16 pixel high font, needs ~3534 bytes in FLASH, 96 characters
#define LOAD_FONT4  // Font 4. Medium 26 pixel high font, needs ~5848 bytes in FLASH, 96 characters
#define LOAD_FONT6  // Font 6. Large 48 pixel font, needs ~2666 bytes in FLASH, only characters 1234567890:-.apm
#define LOAD_FONT7  // Font 7. 7 segment 48 pixel font, needs ~2438 bytes in FLASH, only characters 1234567890:-.
#define LOAD_FONT8  // Font 8. Large 75 pixel font needs ~3256 bytes in FLASH, only characters 1234567890:-.
#define LOAD_GFXFF  // FreeFonts. Include access to the 48 Adafruit_GFX free fonts FF1 to FF48 and custom fonts
#define SMOOTH_FONT
#define SPI_FREQUENCY  27000000
#define SPI_READ_FREQUENCY  20000000
#define SPI_TOUCH_FREQUENCY  2500000
------- TFT_eSPI User Setup Select

#ifndef USER_SETUP_LOADED //  Lets PlatformIO users define settings in
//  platformio.ini, see notes in “Tools” folder.
#include <User_Setups/Setup66_XIAO_Round_Expansion.h>    // Setup file for XIAO serial with GC9A01
#endif // USER_SETUP_LOADED
#define TFT_BGR 0   // Colour order Blue-Green-Red
#define TFT_RGB 1   // Colour order Red-Green-Blue
#define PIN_D0  16  // GPIO16       WAKE
#define PIN_D1   5  // GPIO5        User purpose
#define PIN_D2   4  // GPIO4        User purpose
#define PIN_D3   0  // GPIO0        Low on boot means enter FLASH mode
#define PIN_D4   2  // GPIO2        TXD1 (must be high on boot to go to UART0 FLASH mode)
#define PIN_D5  14  // GPIO14       HSCLK
#define PIN_D6  12  // GPIO12       HMISO
#define PIN_D7  13  // GPIO13       HMOSI  RXD2
#define PIN_D8  15  // GPIO15       HCS    TXD0 (must be low on boot to enter UART0 FLASH mode)
#define PIN_D9   3  //              RXD0
#define PIN_D10  1  //              TXD0
#define PIN_MOSI 8  // SD1          FLASH and overlap mode
#define PIN_MISO 7  // SD0
#define PIN_SCLK 6  // CLK
#define PIN_HWCS 0  // D3
#define PIN_D11  9  // SD2
#define PIN_D12 10  // SD4
--------- Libraries

Using library TFT_eSPI at version 2.5.22 in folder: C:\Users\user\Documents\Arduino\libraries\TFT_eSPI
Using library SPI at version 2.0.0 in folder: C:\Users\user\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.11\libraries\SPI
Using library Wire at version 2.0.0 in folder: C:\Users\user\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.11\libraries\Wire
Using library FS at version 2.0.0 in folder: C:\Users\user\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.11\libraries\FS
Using library SPIFFS at version 2.0.0 in folder: C:\Users\user\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.11\libraries\SPIFFS
Using library Seeed Arduino Round display at version 1.0.0 in folder: C:\Users\user\Documents\Arduino\libraries\Seeed_Arduino_Round_display
Using library lvgl at version 8.3.4 in folder: C:\Users\user\Documents\Arduino\libraries\lvgl

Some other info

ESP32 Chip model = ESP32-S3 Rev 0
This chip has 2 cores
Chip ID: 7773948

Hi there,
So progress none the less, i sent you a message , feel free to past it here..
Stay with it , you’ll get and you are close.
:+1:

GL :slight_smile: PJ :v:

Uncomment that line and build again, come back , let us know.

I only got this far thanks to PJ’s messages on this forum, so thank you very much for all your contributions. Here’s what helped me, in case it can help someone else:

Load and look at this thread, can you complete the steps listed modify the User_Setup_Select.h file and that is 50% of the battle , understanding you can only select the seeed version or Generic driver and separate touch screen driver. the seeed one has both.
I won’t go into why one would use the second option, suffice to say it is available.

The BSP, Board Support package, for this it’s important to use the ones listed in the compiler outputs in all of the code examples. It is that combo that is the secret sauce to getting it working and even the order in which you load the LIB’s will effect soe configurations (resource allocation, i2c, SPI,the begins can conflict, explicitly defining begin params will get you around that also)

and just to show the potential, his amazing ROLO clone :smiley: Code HERE

———–

This line #include <User_Setups/Setup66_XIAO_Round_Expansion.h> looks commented but its not, just some weird copy and paste formatting

What’s the exact model of the boad? XIAO S3? DevKitC-1 or something else?

HI there,

So have you tried these , they will provide a proof of life at a minimum. :+1:

you may find the info valuable. and the precompiled bin. flash it and see if your good. then work backwards, come back and Lmk

HTH
GL :slight_smile: PJ :v:

Hey there,

Sorry I was away for couple of days, the board is a Xiao S3.
I really think there is something wrong with the board, just ordered a couple of board and displays, just to make sure.
I’ll try to compile with these new libraries in the next 2 or 3 days.

Thanks so much.

Just out of interest, how far have you actually managed to get with this development?

I ask as another user is wanting some information on how to get the XIAO ESP32-S3 + Round Display working so was looking at sending them here to start…

Hey,

After almost 10 business days, my new board and display finally arrived. It turned out the issue was caused by bad soldering on the ESP32-S3. The new board worked perfectly, and the old display was fine too.

I also found that if you want to do anything more “heavy” or advanced with it, it’s much better to use PlatformIO. It makes programming and dependency management a lot easier. Additionally, if you want to get the most out of the display, I’d recommend using LovyanGFX instead of TFT_eSPI.

I’ll leave here a basic example I made to test the display

#include <Arduino.h>
#define LGFX_USE_V1
#include <LovyanGFX.hpp>

class LGFX_XIAO_Round : public lgfx::LGFX_Device {
  lgfx::Panel_GC9A01  _panel_instance;
  lgfx::Bus_SPI       _bus_instance;
  lgfx::Touch_CHSC6X  _touch_instance; 

public:
  LGFX_XIAO_Round(void) {
    { // SPI
      auto cfg = _bus_instance.config();
      cfg.spi_host = SPI2_HOST;
      cfg.spi_mode = 0;
      cfg.freq_write = 40000000;
      cfg.pin_sclk = 7;     // D8
      cfg.pin_mosi = 9;     // D10
      cfg.pin_miso = 8;     // D9
      cfg.pin_dc   = 4;     // D3
      _bus_instance.config(cfg);
      _panel_instance.setBus(&_bus_instance);
    }

    { // Painel LCD
      auto cfg = _panel_instance.config();
      cfg.pin_cs           = 2;    // D1
      cfg.pin_rst          = 3;    // D2 
      cfg.panel_width      = 240;
      cfg.panel_height     = 240;
      cfg.invert           = true;
      cfg.rgb_order        = false; 
      _panel_instance.config(cfg);
    }

    { // Touch (CHSC6X)
      auto cfg = _touch_instance.config();
      cfg.x_min      = 0;
      cfg.x_max      = 239;
      cfg.y_min      = 0;
      cfg.y_max      = 239;
      cfg.pin_sda    = 5;     // D4
      cfg.pin_scl    = 6;     // D5
      cfg.pin_int    = 44;    // D7
      cfg.pin_rst    = -1;    
      cfg.i2c_port   = 0;
      cfg.i2c_addr   = 0x2e;  // Not sure if needed - CHSC6X default I2C address
      cfg.freq       = 400000;
      _touch_instance.config(cfg);
      _panel_instance.setTouch(&_touch_instance);
    }
    setPanel(&_panel_instance);
  }
};

LGFX_XIAO_Round display;

void setup() {
  Serial.begin(115200);

  // Backlight ( D6 / GPIO 43)
  pinMode(43, OUTPUT);
  digitalWrite(43, HIGH);

  display.init();
  
  // If weird colors - display.setRotation(2);
  display.setRotation(0); 
  display.fillScreen(TFT_BLACK);
  
  display.setTextColor(TFT_WHITE);
  display.setTextSize(2);
  display.setTextDatum(middle_center);
  display.drawString("Touch CHSC6X OK!", 120, 120);
}

void loop() {
  uint16_t x, y;

  if (display.getTouch(&x, &y)) {
    display.fillCircle(x, y, 10, TFT_GREEN);
    
    Serial.printf("Touch X:%d Y:%d\n", x, y);
  }
  delay(10);
}

And platformio.ini:

[env:seeed_xiao_esp32s3]
platform = espressif32
board = seeed_xiao_esp32s3
framework = arduino
lib_deps =
    lovyan03/LovyanGFX @ ^1.1.16
monitor_speed = 115200
build_flags =
    -DCORE_DEBUG_LEVEL=0
    -O2

Hi there, thanks for the update. Glad you found the problem and have a working solution.

I ended up using LovyanGFX (with DMA) and gave the display its own core, using LVGL 9.5 and EEZ Studio.