XIAO nrf52840 always 100% battery value

Hi I am using a Xiao BLE NRF 52840 to monitor the analog value of a load cell connected to pin A1. I also need to have access to the value of the supply voltage. I read the value from pin A0. Unfortunately, after disconnecting the USB from the device, the value is always 100%. Battery is connected to gold pins on a back of XIAO BLE NRF 52840. This is most likely because the reference value is the battery value. Is there any way to monitor the value of the battery from which the system is powered? Below is my program code.

#include <ArduinoBLE.h>
BLEService ledService("180A");
BLEByteCharacteristic switchCharacteristic("2A57", BLERead | BLEWrite);
BLEService loadService("9A48ECBA-2E92-082F-C079-9E75AAE428B1");
BLEStringCharacteristic loadLevelChar("2D2F88C4-F244-5A80-21F1-EE0224E80658", BLERead | BLENotify, 20);
BLEService batteryService("180F");
BLEUnsignedCharCharacteristic batteryLevelChar("2A19", BLERead | BLENotify);
const double Freq = 30;
unsigned long Cur_ms_Count;
unsigned long Last_ms_Count;
unsigned long T_ms_Count;
unsigned long millisoffset;
unsigned long zeromillis;
int flaga = 0;
String sText;
void setup() {
  Serial.begin(9600);
  T_ms_Count = 1000 / Freq;
  sText = "";
  Last_ms_Count = 0;

  //while (!Serial)
  //;

  pinMode(LED_BUILTIN, OUTPUT);
  if (!BLE.begin()) {
    while (1)
      ;
  }

  BLE.setLocalName("LoadMonitor");
  BLE.setAdvertisedService(loadService);
  loadService.addCharacteristic(loadLevelChar);
  BLE.addService(loadService);
  BLE.setAdvertisedService(batteryService);
  batteryService.addCharacteristic(batteryLevelChar);
  BLE.addService(batteryService);
  BLE.setAdvertisedService(ledService);
  ledService.addCharacteristic(switchCharacteristic);
  BLE.addService(ledService);

  BLE.advertise();
  Serial.println("Bluetooth device active, waiting for connections...");
}

void loop() {
  BLEDevice central = BLE.central();

  if (central) {

    digitalWrite(LED_BUILTIN, HIGH);

    while (central.connected()) {

      if (switchCharacteristic.written()) {
        switch (switchCharacteristic.value()) {
          case 01:
            flaga = 1;
            break;
          case 02:
            flaga = 2;
            millisoffset = millis();
            break;
          default:
            flaga = 0;
            break;
        }
      }
      while (flaga == 0) {

        break;
      }
      while (flaga == 1) {
        Cur_ms_Count = millis();
        if (Cur_ms_Count - Last_ms_Count >= T_ms_Count) {
          int Battery = analogRead(A0);
          int BatteryLevel = map(Battery, 0, 1023, 0, 100);
          batteryLevelChar.writeValue(BatteryLevel);
          Cur_ms_Count = millis();
          break;
        }
      }
      while (flaga == 2) {
        Cur_ms_Count = millis();
        if (Cur_ms_Count - Last_ms_Count >= T_ms_Count) {
          zeromillis = Cur_ms_Count - millisoffset;
          int Load = analogRead(A1);
          int LoadLevel = map(Load, 0, 1023, 0, 100);
          int Battery = analogRead(A0);
          int BatteryLevel = map(Battery, 0, 1023, 0, 100);
          sText = String(zeromillis) + '\t' + String(LoadLevel);
          loadLevelChar.writeValue(sText);
          batteryLevelChar.writeValue(BatteryLevel);
          Last_ms_Count = Cur_ms_Count;
          break;
        }
      }
    }
    digitalWrite(LED_BUILTIN, LOW);
  }
}

Hi michugroove,
There is a way to do this as described in the 1/44 post in the link below. However, you will need to respond to the 31/44 posting.
“https://forum.seeedstudio.com/t/xiao-ble-sense-mbed-2-7-2-battery-charge-and-voltage-monitor-analogread-p0-31-does-not-work/ 266438”

When using A0 to measure battery voltage normally, the following points should be noted
The battery voltage must be divided below VDD,
The reference voltage for the ADC should be the internal reference voltage. (default is VDD)