Xiao IO expander COMING, and Going.. Roll your own. ✌

MengDu on discord made a good point that made me think, revise the board layout that the board is centered on the base XIAO and bring the pins out on header exactly parallel and offset of XIAO pins, so it would be two parallel rows, the base Xiao pins inside and expansion pins in the outside row… you follow?

Hi there,
I’m Glad they are looking at the whole expansion IO capability, For me as long as they don’t engineer it closed then I think it will be great!
They should always error on the side of MORE not LESS. IMO.
The B2B connector on the XIAO was a Happy day for me to see the possibilities it can lead to and make using Xiao really flexible.

I would be ok with a slight increase ,($1) IF so on the price even though the connector is less than that.
I need 4 or five for a project, but I am NOT buying cameras with them to just chuck in a drawer and never use. They need to either make them with it as is or add a new SKU#
I’ll inquire on the discord as well.

GL :slight_smile: PJ
:v:

Looks like … some flattery from Robot -man…


the one on the left , PLEASE turn to your right… I’m sure I have seen you somewhere else… LOL
see they know a good idea when they see it…
GL :slight_smile: PJ :v:

as you were. :+1:

we need a wow emoji here… sometimes heart doesnt cut it…

Hi, Seeed, this IO expander is not just out of stock, the page is 404: https://www.seeedstudio.com/GPIO-Expander-for-XIAO-p-5795.html

Has it been discontinued entirely?

that device was experimental… something must have happened with the owner of the design or something because it never went into production… usually seeed does not remove wiki information for archival reasons… which is great so i think something happened on this thing… but anyway… its good to get the feedback, it may be reincarnated.

Hi there,

So to Put a :wrapped_gift: on this one…

Seeed is Offering the (good move IMO) this ;

WHY is it Great ?

:grin:

You need to look just a little closer at some often over looked finer points to see why this XIAO ESP32 is a Sleeper…

  1. On-chip 8MB PSRAM & 16MB Flash
  2. 1x B2B Connector
  3. Charging current: 100mA(Fast) / 0.9mA(Trickle)
  4. 2x SPI
  5. Light Sleep 2.54ma @3.8Vdc

Adding IO, is a SNAP :hand_with_index_finger_and_thumb_crossed: :smiling_face_with_sunglasses:
We get plenty O sun here in SOFlo… with a High Quality Battery..

and a Crappy/Cheapy Solar Panel :backhand_index_pointing_left: :face_with_open_eyes_and_hand_over_mouth: , the Stuff just Works.

It’s NOT a Wearable Battery friendly device @ 33ua. either. unless you like recharging a Thin Round Lipo (every day). Those additional I/O Castellated pins (micro-pins) WHO is gonna use those on Breadboard , LOL how? :face_savoring_food:
The PLUS version is the Only one to buy of the “series” :backhand_index_pointing_left: :face_with_tongue: IMHO
:person_bowing:

As you were,
HTH clear it up
GL :slight_smile: PJ :v: