Hi there,
I went back and checked my working demo, I used the original esp32by Espressif systems 2.0.8. , tried the other all the way to the Alpha 's 3.0.0 .
Would not compile with 2.0.10 (wifi errors with wifi 2.0 lib)nor with the Alpha’s 3…0.0 a1 or a2
Works with 2.0.14 fine.
compiler snip below
HTH
GL
PJ
Successfully created esp32s3 image.
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.14/tools/gen_esp32part.exe" -q "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B02CDFCE65CF503472EE9E89E2619EE2/partitions.csv" "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B02CDFCE65CF503472EE9E89E2619EE2/CameraWebServer_copy_PJ.ino.partitions.bin"
cmd /c if exist "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B02CDFCE65CF503472EE9E89E2619EE2\\libraries\\Insights" "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.14/tools/gen_insights_package.exe" "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B02CDFCE65CF503472EE9E89E2619EE2" CameraWebServer_copy_PJ.ino "D:\\Arduino_projects\\CameraWebServer_copy_PJ"
cmd /c IF 0==1 COPY /y "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\tools\\openocd-esp32\\v0.12.0-esp32-20230419\\share\\openocd\\scripts\\board\\esp32s3-builtin.cfg" "D:\\Arduino_projects\\CameraWebServer_copy_PJ\\debug.cfg"
cmd /c IF 0==1 COPY /y "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.14\\tools\\ide-debug\\esp32s3.json" "D:\\Arduino_projects\\CameraWebServer_copy_PJ\\debug_custom.json"
cmd /c IF 0==1 COPY /y "C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\hardware\\esp32\\2.0.14\\tools\\ide-debug\\svd\\esp32s3.svd" "D:\\Arduino_projects\\CameraWebServer_copy_PJ\\debug.svd"
Using library WiFi at version 2.0.0 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.14\libraries\WiFi
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\tools\\xtensa-esp32s3-elf-gcc\\esp-2021r2-patch5-8.4.0/bin/xtensa-esp32s3-elf-size" -A "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\B02CDFCE65CF503472EE9E89E2619EE2/CameraWebServer_copy_PJ.ino.elf"
Sketch uses 788857 bytes (23%) of program storage space. Maximum is 3342336 bytes.
Global variables use 59208 bytes (18%) of dynamic memory, leaving 268472 bytes for local variables. Maximum is 327680 bytes.
"C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\tools\esptool_py\4.5.1/esptool.exe" --chip esp32s3 --port "COM23" --baud 921600 --before default_reset --after hard_reset write_flash -z --flash_mode dio --flash_freq 80m --flash_size 8MB 0x0 "C:\Users\Dude\AppData\Local\Temp\arduino\sketches\B02CDFCE65CF503472EE9E89E2619EE2/CameraWebServer_copy_PJ.ino.bootloader.bin" 0x8000 "C:\Users\Dude\AppData\Local\Temp\arduino\sketches\B02CDFCE65CF503472EE9E89E2619EE2/CameraWebServer_copy_PJ.ino.partitions.bin" 0xe000 "C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.14/tools/partitions/boot_app0.bin" 0x10000 "C:\Users\Dude\AppData\Local\Temp\arduino\sketches\B02CDFCE65CF503472EE9E89E2619EE2/CameraWebServer_copy_PJ.ino.bin"
esptool.py v4.5.1
Serial port COM23
Connecting...
Chip is ESP32-S3 (revision v0.2)
Features: WiFi, BLE
Crystal is 40MHz
MAC: 84:fc:e6:6a:d0:f0