XIAO-ESP32-S3 with ST7789 1.22" display

Hi there,

SO, you mean the REAL DEV modules like this one.




This is a C6 , but full monty..:+1:

They are different from a XIAO a lot different. (cores are the same is about it)… :face_with_hand_over_mouth:
The big boys are pinned the same , so probably why they both work, It’s the Pins and config, We will get it , no worries.
Can you post the compiler output First 3 lines(be sure your prefs are set to Verbose Output) post it up with the last 15 , right before it uploads. :v:

HTH
GL :slight_smile: PJ :v:

meanwhile, look over this post
Round Display with Xiao C3, C6, S3 & S3-Plus Test Examples - #3 by PJ_Glasso
:+1:
GC9A01 and Xiaio esp32 - #30 by BRW_MASTER

1 Like