Dear Staff
I recently purchased a RUNBER FPGA Development Board via Digikey.
The board looks different than the photos on the product pages.
On the backside the Board is marked:
MINI EYE BOARD GWIN V1.2
20210618
And it has a 20 pin WCH CH552T uart chip. instead of the FT232 shown on all schematics I can find.
Also its not straightforward to find the RUNBER FPGA Development Board on Seed Studios web pages, and the product page shows data on V1.1 and not V1.2 ?
Best wishes Michael
If the RUNBER FPGA Development Board Ver. 1.2 exists, the schematic and related documentation are typically provided by the manufacturer or vendor of the development board. You can try the following steps to locate the schematic:
Visit the official website of the manufacturer or vendor of the RUNBER FPGA Development Board. Look for a dedicated product page or technical documentation section that might include the schematic and related resource foxynamer.
If you can’t find the schematic on their website, consider reaching out to the manufacturer or vendor directly. They may provide you with the required documentation upon request or direct you to the appropriate resources.
Thanks for your reply @Tatum45
Quoting from where I purchased the board:
Manufacturer Seeed Technology Co., Ltd
This forums owner should be the manufacturer.
Since my board was unable to utilize the embedded flash I have been in contact with seen technical
support and they have verified that its a V1.2 board with a well known hardware defect and that they are willing to ship a new board via my distributor.
Here is Seeds link to the V1.1 product and schematic:
Here is an image of the backside of my V1.2 product for comparison:
I recommend you to contact Digikey’s customer support for clarification on the product version you have received as well as difference from the product page.https://capcutmods.org/ Also you may want to get in touch with the Seed Studios to inquire about the version update and any relevant documentation for the V 1.2 board.
If you can’t find the schematic online or in the product documentation, consider contacting the manufacturer’s customer support or technical support for assistance. They may be able to provide you with the schematic or direct you to the right resources.
Beware of Third-Party Documentation: Sometimes, third-party websites or documentation repositories may have the schematic for development boards. Be cautious about the source and ensure it’s a reliable and trustworthy one.
Regards:
Tierbestattung Albstadt
It appears that the Runber FPGA Development Board V1.2 is a slightly different version of the V1.1 board, but it should still be a functional development board that you can use to run FPGA applications.
Welcome to Hotel Ardeche, where adventure meets relaxation in the heart of breathtaking landscapes. Experience the cool vibe of our charming retreat, where every moment is filled with warmth and hospitality.
Visit the official website or support page of RUNBER or the manufacturer of the FPGA development board. They may have documentation, schematics, and other resources available for download and also User Manuals and Documentation**: Check any user manuals, datasheets, or Salary Calculator that came with the FPGA development board. Schematics are often included in these resources.
@itstonystark
Amazing information Thanks for this I will share this on WhatsApp with my community.
Dear [@Michael_Brown ]
I recently purchased a RUNBER FPGA Development Board through Digi-Key, and I’ve noticed some discrepancies between the board I received and the product description.
Specifically, the board I received is marked on the backside with the following:
- MINI EYE BOARD GWIN V1.2
- 20210618
Additionally, it features a 20-pin WCH CH552T UART chip, whereas all the schematics I have found indicate that the board should be equipped with an FT232 chip.
Furthermore, I’ve had difficulty locating detailed information about the RUNBER FPGA Development Board on Seed Studio’s website, particularly regarding the V1.2 version. The product page I found only seems to provide information on V1.1, not V1.2.
Could you please clarify these differences and provide the correct documentation or schematics for the version of the board I received?
Thank you for your assistance.
Best wishes,
Mobile patrol security services
Thanks for the information Chris I will share this info with my community in Call Packages
- Board Version Differences: It’s common for development boards to go through various revisions, and it seems like you received a newer version (Pre cana course) that might have slight differences from the V1.1 version documented online. The change from an FT232 to a WCH CH552T UART chip could be a part of this revision.