Using the “Wio-SX1262 for XIAO” to easily build LoRa point-to-point communication with various XIAOs

Hi there,

Ok, So you miss understood.
The pins defined in the demo are for the B2B version of the lORA board, You are using the First revision Board for XIAO.
So those pins are incorrect for that version of lora board.

Change them to the GPIO numbers of the silk-screen ) number D1-D10.
Look at the pictures again. I have the GPS board on there, Here is a thread that goes more deeply into the discussion but the pins are more aplicable.

something along theses lines,

SX1262 radio = new Module(/*NSS*/D4, /*DIO1*/D1, /*NRST*/D2, /*BUSY*/D3);

from this :crossed_fingers:

SX1262 radio = new Module(41, 39, 42, 40);  // NSS, DIO1, RST, BUSY

HTH
GL :slight_smile: Pj :v:

you have this one.


You may NOT have PIN 6 though, some boards did not have that connection. :+1:

1 Like