A point-to-point long distance communication experiment was carried out with XIAO_MG24 mounted on Wio-SX1262 for XIAO. The main parameters are: frequency 922.6[MHz], Txpower=13[dBm], bw=125[kHz], sf=12, cr=5, antenna λ/2.
Stable communication was achieved with RSSI=-127[dBm] and SNR=-15[dB] over a line of sight of 24.5[km].
This was the same as the results of the experiment with LoRa-E5 mini shown in the link below.
Here is the sketch I used for the experiment. The sketch should be easily modified for other XIAOs.
POST_SX1262_MG24_P2P.zip (8.5 KB)