Jetson Orin NX (Seeed A603) header UART not receiving PX4 TELEM2 — USB-TTL (3-wire) works, onboard UART silent
Setup
- Flight controller: CubePilot Cube Orange Plus
- Autopilot: PX4 v1.16.0
- Companion: Jetson Orin NX 16 GB on Seeed reComputer A603
- OS/SDK: JetPack 6.2 (Ubuntu 22.04)
- Tools available: QGroundControl, MAVProxy, mavlink-router, PyMAVLink, Micro XRCE-DDS Agent v2.4.2
- Wiring (A603 W8 ↔ TELEM2, 3.3 V TTL):
- A603 pin 8 (UART1_TX) → TELEM2 pin 3 (RX)
- A603 pin 10 (UART1_RX) ← TELEM2 pin 2 (TX)
- GND ↔ GND (TELEM2 pin 6)
- (Also tried RTS/CTS on A603 pin 11 ↔ TELEM2 CTS and A603 pin 36 ↔ TELEM2 RTS)
Goal / Modes
- MAVLink over TELEM2 → Jetson
MAV_1_CONFIG=TELEM2
,SER_TEL2_BAUD=230400
and921600
,MAV_1_MODE=Onboard
,UXRCE_DDS_CFG=Disabled
- uXRCE-DDS over TELEM2 → Jetson
MAV_1_CONFIG=Disabled
,UXRCE_DDS_CFG=TELEM2
, same baud rates; Jetson runsMicroXRCEAgent serial -D <port> -b <baud>
What works (baseline)
- Using a USB-to-TTL 3.3 V dongle on Cube TELEM2 (→
/dev/ttyUSB*
), both MAVLink and uXRCE-DDS work at 230400 and 921600. - This working case uses only GND, TX, RX (no RTS/CTS).
What doesn’t work
- Using the A603 40-pin header UART on the Jetson (expected
/dev/ttyTHS1
), I get no data. - Already disabled
[email protected]
andModemManager
. - Tried line settings with and without HW flow control, e.g.:
stty -F /dev/ttyTHS1 230400 cs8 -cstopb -parenb -ixon -ixoff -crtscts
stty -F /dev/ttyTHS1 921600 cs8 -cstopb -parenb -ixon -ixoff -crtscts
- Raw reads show nothing; moving the exact same TELEM2 cable back to a USB-UART dongle works immediately.
Asking for help
- What is the correct
/dev/tty*
mapping for the A603 W8 header UART on Orin NX + JetPack 6.2? Is itttyTHS1
or another node? - Is there a known-good device-tree overlay or jetson-io recipe to enable that header UART (and RTS/CTS) on the A603?
- Any known quirks at 921600 on this header that require flow control or specific termios settings on Orin NX?
- Besides ModemManager/getty, are there other services on JP 6.2 that commonly grab THS UARTs?
- If someone has Cube TELEM2 ↔ A603 header UART working, could you share which
/dev/tty*
, whether RTS/CTS is enabled, and the baud/flow-control settings that were stable?
Thanks in advance—happy to apply any suggested overlay/config and report back the exact working recipe.