🔋 The Battery...Which Xiao and Why?

The Battery…Which Xiao and Why?

:battery: Choosing the Right Battery for Your Xiao Board

Battery selection is crucial when working with Seeed Studio’s Xiao series. Factors like charging chip differences, power profiling, and project needs will determine the best choice. This document outlines the differences across Xiao boards and considerations for selecting the best battery.


:high_voltage: Key Factors in Battery Selection

  1. Battery Chemistry & Voltage

    • Most Xiao boards support 3.7V or 3.85V LiPo batteries.
    • Built-in over/under voltage protection is ideal for safety.
    • Different battery shapes: Round, Square, Flat—which one fits your project?
  2. Charging Chip & Current Ratings

    • Different Xiao boards use different charge controllers, affecting charge speed and battery compatibility.
    • Some charge ICs are configurable, while others have fixed charge rates.
  3. Power Profiling & Runtime Estimation

    • Power consumption varies by board. Measuring active vs. deep sleep current is key.
    • Online tools like Digikey’s Battery Life Calculator can help predict runtime.

:magnifying_glass_tilted_left: Xiao Board Battery Charging Comparison

Xiao Board Charging Chip Max Charge Current Recommended Battery Power Considerations
Xiao nRF52840 TP4054 50mA (default), configurable to 100mA 3.85V 450mAh LiPo (Round/Square) Best for low-power applications, BLE projects.
Xiao ESP32C3 TP4057 100mA 3.7V 500mAh+ LiPo (Flat/Square) More power-hungry due to WiFi, benefits from larger battery.
Xiao ESP32S3 TP4057 100mA 3.7V 500mAh+ LiPo Dual-core processor increases power draw; power profiling is recommended.
Xiao ESP32C6 TP4057 100mA 3.7V 450-600mAh LiPo Lower power than ESP32S3, but still benefits from optimized battery selection.

:wrench: Power Profiling & Optimization

  • Measure current consumption in different modes (active, sleep, deep sleep) before finalizing a battery choice.
  • Use tools like the Digikey Battery Life Calculator to estimate runtime based on power draw.
  • Consider adding external power management circuits for efficiency.

:speech_balloon: Discussion & Community Input

  • What battery do you use with your Xiao board?
  • Have you tested different charge rates or power optimizations?
  • Do you prefer round, flat, or square LiPo batteries for your projects?

—let’s open up the discussion! :rocket:

Hi PJ,
The information on the ESP32C3 charge controller seems to be different from earlier lots. Have you confirmed this in any way?

Hi there,

Ah’ good catch, I have tried I knew it looked to clean, only the older schematic had it called out, the new one is missing? I re-checked the same. I will inquire also on the discord and see if they reply. Perhaps Kevin could tell us if this is the case. I think the first pcs i tested had a lower current, but it was a while back so I 'm betting they changed it after the chip shortage situ. ? But EAGLE eye as per usual My guy… :+1: What batteries have you used and had success with? I’m sure you got the receipts. :grin:

GL :slight_smile: PJ :v:

The three ESP32C3s I got two years ago had a charge current of 370mA.
The drawings do not list the name of the charge controller, so I do not know what is actually mounted on the more recent C3s.

Hi there,

Yea, I’ll take you WORD on that, I thought the earlier ones were indeed different, got it backwards more than likely. We even had a few post I think others may have noticed. Probably wouldn’t be the first time with the supply and demand waves. I want them to use a PMIC, one that’s connected via I2C really do the Xiao thing right. replace the boot button as a power push button (connected to the pmic) with a MCUBoot Loader they can, ALL xiao’s just one button. Then USE the corners of the board as TOP-SIDE Battery PADS.
like this: (in Seeed Green)

It would work on every Xiao except the nrf52840 Sense version because some PCB cowboy :cowboy_hat_face: put a resistor WAY out on the edge (DRC_check FaiL ) past the PDM. so they would have to fix that.
Look with a magnifier a single resistor. I’m sure I could find it on the Schematic and BOM. Sure beats POGO pins… Wait until you see the next video…LOL

Thanx for the contribution as always.
GL :slight_smile: PJ :v:

as powerful as these batteries are, we are talking about basicly delta 1 volt between charged and XIAO brownout 4.2 v to 3.2 v

Do you know if it is possible to limite the charging voltage to a specific voltage?
I have a few meshtastics solar nodes with large batteries that I would like to keep the voltage bellow 4V.

Thank you!

i think the charging chip is “dumb” it has no logic to manipulate to change any settings

Hi there,

So , Only the Charge current is manageable, two choices P0.13 HICHRG Pin 20ma. or 100ma.
Here is a link with code if that is helpful :+1:

HTH
GL :slight_smile: PJ :v:

I’m using the Xiao ESP32S3 and Wio SX1262 module kit. Previously, I used a 1200mAh battery and charged it directly using the board.

Then, when I changed the battery to 1800mAh, it never fully charged, only staying at around 4 volts. Is this normal?

Hi there,

And Welcome Here.

So , some of the batteries and even some charge banks , the Xiao doesn’t present a large power draw , and they shut off. I see some batteries need a higher charge current, even though they are labeled for a 1C Charge rate, it may need a little more, some Xiao’s you can set it to one of two currents.

HTH
GL :slight_smile: PJ :v:

to test i will also plug in a cell phone to provide a baseload

Excellent info. Bookmarking this !

Good Job Brother! You are Leveling up Quick!

Hi All

Great thread and very useful thanks. I saw that the charge current for the ESP32C3 could be 370ma Vs the 100ma in the initial table. Is anyone able to confirm whether the ESP32C6 is definitely 100ma please? I have a 300maH LiPo for my project so concerned that if the current is potentially the same as the ESP32C3 that would be too much - battery is rated at 1 C

Many thanks in advance

Lee.

In case it helps others, after digging around I found this schematic diagram ( https://files.seeedstudio.com/wiki/SeeedStudio-XIAO-ESP32C6/XIAO_ESP32_C6_v1.0_SCH_260114.pdf). Looks like the charger is a SGM40567-4.2XG and has a 200k resistor between C1 and GND so charging current is 120mA.