ESP32-C3 XIAO Battery Charging IC

Does anyone know the IC used for for the battery charging circuit?
The schematic just labels it as U1 and does not give a part number.

I want to use a secondary 4.5V power supply (not a battery) to power the board when USB is not plugged in, so I planned on connecting it to the battery pads. This is higher than a battery’s typical voltage, so I just want to make sure it’s safe to do so. The 3.3V LDO regulator circuit looks like it would work with a 4.5V power supply, but I can’t confirm that the battery charging circuit won’t explode when 4.5V is applied to the battery voltage because I don’t know what IC it is.

Any help would be greatly appreciated.

Hi @melsh
The IC used for for the battery charging circuit(U1) is ETA4054

Do you know if it’s safe to simultaneously plug in the GND/5V pins and the USB to charge a lipo battery ?

On the Seeed Studio XIAO ESP32C3, it is generally safe to use both the USB connection and the 5V pin at the same time.

This includes:

  • having the USB cable plugged in, and

  • supplying 5V through the 5V pin.

You can do this while a LiPo battery is connected and charging.

The external 5V supply should be well regulated. It should also stay close to standard USB voltage, around 5V.

Since this connects the outputs of two 5V power sources, it could cause a malfunction depending on the type of power source connected. I do not recommend supplying power to both the USB and 5V pins at the same time.

Hi there,

So , “NO” would be the correct answer. Generally or otherwise. Have a Look at the Schematic, you will see where two power paths and the potential for a conflict , source or SInk. so, NO. it is never advised and is not listed in the wiki or technical documentation any where, quite the contrary.

HTH
GL :slight_smile: PJ :v:

@PJ_Glasso If the power supply is regulated, still No?

If there is a way to prevent feed back from XIAO’s Pin 5V to USB 5V or vice versa then no :cross_mark:. Otherwise there could be an issue.

Since the USB 5V (voltage) can’t be controlled (depends on USB), the easiest way is to have the “regulated” 5V include a series diode/MosFET and be a lower voltage than the USB’s 5V (eg 4.5V - I have some USB hubs that can only supply 4.7V).

Hi there,

So , @grobasoz has it right..
Maybe if you use some Zener diode clamp type config, but it’s just not worth it technically IMO.

man , take a week off to bury my mom in PA. and the questions pile up, fazoul I got 38 emails..:grin:

GL :slight_smile: PJ :v: