yes you dont need to wipe the flash first. did you do the reset procedure? press the button and “double click” the magnetic connector on and off real fast
[Flashing Meshtastic on the WIO Tracker 1110 from Seeed Studio]
Flashing Meshtastic on the WIO Tracker 1110 from Seeed Studio.
I purchased the WIO Tracker 1110 from Seeed Studio when it was first introduced. I haven’t developed a use case until Seeed Studio developed an OLED display and compatible GPS to make the WIO Tracker compatible with Meshtastic. So I work out what I need to do to flash Meshtastic on the WIO Tracker 1110 and put it to the test.
Key is to cd to the directory …
different device but same procedure