Flashing Meshtastic on the WIO Tracker 1110 from Seeed Studio.
I purchased the WIO Tracker 1110 from Seeed Studio when it was first introduced. I haven’t developed a use case until Seeed Studio developed an OLED display and compatible GPS to make the WIO Tracker compatible with Meshtastic. So I work out what I need to do to flash Meshtastic on the WIO Tracker 1110 and put it to the test.
Key is to cd to the directory holding adafruit-nrfutil.exe
C:\Users\cgwal\AppData\Local\Packages\PythonSoftwareFoundation.Python.3.13_qbz5n2kfra8p0\LocalCache\local-packages\Python313\Scripts
also key is to add .\ infront of the command!
success is when the drive name changes from boot to WM1110_BOOT