I reload, now doesn’t work. It looks like we missed a step here? All the libraries are the correct versions, the setup files look correct. The only delta I can find is the space used for global variables?
Was there another step we did that I forgot to document? It now repeatly crashes again and again…
Creating esp32c3 image...
Merged 2 ELF sections
Successfully created esp32c3 image.
python3 /Users/localuser/Library/Arduino15/packages/esp32/hardware/esp32/2.0.17/tools/gen_esp32part.py -q /private/var/folders/sc/4y094kzs1rs26_qzh6wfr5qr0000gp/T/arduino/sketches/D2021C59B7223DD82C9812977605CDBE/partitions.csv /private/var/folders/sc/4y094kzs1rs26_qzh6wfr5qr0000gp/T/arduino/sketches/D2021C59B7223DD82C9812977605CDBE/demo.ino.partitions.bin
/usr/bin/env bash -c "[ ! -d \"/private/var/folders/sc/4y094kzs1rs26_qzh6wfr5qr0000gp/T/arduino/sketches/D2021C59B7223DD82C9812977605CDBE\"/libraries/Insights ] || python3 \"/Users/localuser/Library/Arduino15/packages/esp32/hardware/esp32/2.0.17\"/tools/gen_insights_package.py /private/var/folders/sc/4y094kzs1rs26_qzh6wfr5qr0000gp/T/arduino/sketches/D2021C59B7223DD82C9812977605CDBE demo.ino \"/Users/localuser/Arduino/demo\""
Using library TFT_eSPI at version 2.5.23 in folder: /Users/localuser/Arduino/libraries/TFT_eSPI
Using library SPI at version 2.0.0 in folder: /Users/localuser/Library/Arduino15/packages/esp32/hardware/esp32/2.0.17/libraries/SPI
Using library FS at version 2.0.0 in folder: /Users/localuser/Library/Arduino15/packages/esp32/hardware/esp32/2.0.17/libraries/FS
Using library SPIFFS at version 2.0.0 in folder: /Users/localuser/Library/Arduino15/packages/esp32/hardware/esp32/2.0.17/libraries/SPIFFS
Using library Seeed Arduino Round display at version 1.0.0 in folder: /Users/localuser/Arduino/libraries/Seeed_Arduino_Round_display
Using library lvgl at version 8.3.7 in folder: /Users/localuser/Arduino/libraries/lvgl
Using library Wire at version 2.0.0 in folder: /Users/localuser/Library/Arduino15/packages/esp32/hardware/esp32/2.0.17/libraries/Wire
/Users/localuser/Library/Arduino15/packages/esp32/tools/riscv32-esp-elf-gcc/esp-2021r2-patch5-8.4.0/bin/riscv32-esp-elf-size -A /private/var/folders/sc/4y094kzs1rs26_qzh6wfr5qr0000gp/T/arduino/sketches/D2021C59B7223DD82C9812977605CDBE/demo.ino.elf
Sketch uses 286070 bytes (21%) of program storage space. Maximum is 1310720 bytes.
Global variables use 14164 bytes (4%) of dynamic memory, leaving 313516 bytes for local variables. Maximum is 327680 bytes.