Hi
I recently purchased a Orin 16GB and was able to flash 6.0 using SDK Manager (Host Ubuntu 22.04 LTS) successfully. After rebooting the Orin device, the Host machine no longer identifies the Orin device connected to the Host (using the Data cable) neither in the SDK manager nor through lsusb cmd.
Need help and directions on how to resolve this USB issue and flash the Orin for the following.
- Jetson SDK: JetPack 5.1.1
- Version: JetPack 5.1
Thanks in advance.
This is similar to
https://forum.seeedstudio.com/t/recomputer-j4012-orin-nx-16gb-usb-c-port-stopped-working-after-flashing-with-jetpack-5-1-2/271738