reComputer J401 - support for Super Mode

Hi, sorry for the delayed reply.

  1. Currently, the carrier boards that support Super Mode include our Robotics J401 Carrier Board and Mini Carrier Board, among others. You can find these products via the link below. All of them come with the v6.2 version image, which can be upgraded to Super Mode.

reComputer Robotics J401 carrier board of NVIDIA® Jetson™ Orin™ NX/Orin™ Nano

NVIDIA® Jetson Orin™ NX/Nano mini carrier board

  1. We will also launch a new Super Mode-compatible carrier board in Q1 next year – feel free to keep an eye out for it.
  2. The circuit diagrams and related documentation for these carrier boards are all open-source.

Thank you for your interest.

Hi Lorraine,

I have been reading this thread, as much as I understand of it. I am a newbie with the J3011 as well as Linux and nVidia. I have been trying to set up my J3011 for Super mode for the past 2 months and have not been successful. I have gotten to the point of the beginning of this thread and flashed the J3011 again, with Jetpack 6.2. Still no MAXN SUPER mode.

Can you help? Thank you very much in advance. Best wishes for 2026.

hey @seeed_lorraine

Thats great! Thanks for the clarification.

If you could, please update the page below to include the orin nx compatible jetpack 6.2 images. That would make it alot easier for us to upgrade to 6.2.
link::wiki.seeedstudio.com/recomputer_jetson_mini_getting_started/

Thanks!

Alan

Hi, yes, you can send an email to [email protected]. Please attach the output result of the command “cat /etc/nv_tegra_release” to the email. We will help you troubleshoot the issue.

Hi, we apologize, but currently, the Mini version 6.2 is only available for the Orin Nano. For the Orin NX, the fan may not provide sufficient support for operation in Super mode. You can wait for our new Super carrier board to be launched.

Noticed yesterday that a new heatsink was released: “Aluminum Heatsink with Fan for Jetson Orin Module Super Mode” Link to store: Fan for NVIDIA® Jetson Orin™ Super mode

Do we need a completely new carrier board, or simply switching the heatsink & fan will be enough on the existing J4012 (non super) board?

Hi afsyd, this Super cooler is part of our Super series kit. Its interface is 12V, while the fan interface of the J30/J40 carrier board is 5V, so they are not compatible. We recommend that you purchase a brand-new Super carrier board as a replacement.

Hi, so is there any drop in replacement board for reComputer J4012?
I just want to upgrade my setup to use SUPER mode, but I dont need that extra stuff that comes with industrial/robotics packages.

Hi, this carrier board is recommended for purchase, and it supports Super mode.