I can’t seem to post to the “Arduino & Seeeduino” forum. When I click ‘submit’, it just seems to reload the page.
well. this is odd. Once I posted here, it let me post in the other section.
Forums are platforms where people hold a discussion on particular topics. Let’s understand the meaning of the term Forum Posting. A place or medium where ideas are exchanged that helps in knowledge.It can be considered as publishing your ideas on the forum Collectively we can say that this is a way through which we post comment our suggestions and views.
however it does not work, may be negative statements are filtered?
hey, same here. can’t find a button to start a new topic
you have to level up by looking at posts
my recomendation is to look at some posts and heart a few.. even if you dont REALLY LOVE THEM and then you will level up soon… i know this is a pain for new users who want to just ask a question but that is the way it is if you see a post that is close to what you are asking you can reply to that post
DO NOT POST TO RANDOM THREADS
Do not post on any random thread to get your question out before leveling up.
Your post and account may be deleted for violation of this policy.
It is ok if you searched and found an applicable thread to your question… but dont post a support question on a how to bake a cake thread… follow my drift? This is starting to be a problem
Commenting here to see if I can create a topic after making this post.
Hi there,
And Welcome here…
SO it’s a spam protection, you need to level up by commenting or posting on an existing thread, Most Forums these have a " Introduce yourself " for the same reason. This one is big enough they could look to that method as well. After you reply or post 3 count I think it is, You can make your own topic and post links , pics, etc.
HTH
GL
PJ ![]()
Commenting to see if I can make a post now.
nope
Does anyone actually know how to make a post? Is there a set limit to how many interactions you have to make before you are allowed? Help??
Hi there,
Get to trust level 1 by…
- Entering at least 5 topics
- Reading at least 30 posts
- Spend a total of 10 minutes reading posts
HTH
GL
PJ ![]()
you may need to define entering for those of us that have dirty minds…
If you cannot create a new topic, love my reply. It may help! ![]()
So they made this forum just as much of a nightmare as it is to try and configure their product. Nvm after looking at some old posts they did have somewhat of a bot problem.
Still can’t post at level 1 though…
Hi there,
And Welcome here I think?
So, What the Product you’re referring to? If you don’t mind get to the point if you need some help. Link or device name to start or perhaps a description of what it is you are having an issue with.
We can help but you’ll need to have a better approach for high Q. and confidence
HTH
GL
PJ ![]()
Actually we run a pretty chill forum here…
not all the drama of the rest of the world and we like it that way
Our housekeeping is a little dirty, we dont close topics for just this reason
anyone can pop on and find a topic they are interested in and comment there
truly there is really no question that has not been asked and answered here
so if you are waiting to level up… search for your answer and you will probably find
Enjoy… if you are here in a month we will consider you a contributor
Hi there,
LOL, Yea, It’s not REDIT ![]()
more of a teach a man to fish
place than , Hand you a sandwich
. It’s good tech and Solid products but they require some attention to detail.
HTH
GL
PJ ![]()
Hi Everyone,
Ive just joined the forum today and would like know if anyone could point me in a direction, I work on an oil field and we use solar lighting however solar lighting attracts thieves, and Id like to build a LoRaWAN GPS which I can solder to the back of a 6V/20Watt solar panel using a 3.7V battery as well to power the LoRaWAN GPS
Hi there,
And Welcome here…
So, Very sorry to hear the motivation for the post and I empathize with your position,it’s not like you don’t have better stuff to keep after , YOI.. ![]()
You may be better served with the t1000 unit ?
Can you dicribe what the end goal would be ?
To track or to just monitor
Operational status?
Lots of smart LoRa capable folks here so. Let it RIP ![]()
HTH
GL
PJ ![]()