WPS is the easiest way to connect… and works well on the Xiao ESP32c3,
I’m using an ARRIS Router with a Hard & Soft WPS button press. AOK
/*
THIS lightly tweeked PJG Example Code To Get ESP32c3 info from chip
 and to Connect WPS button AP and display RSSI, as well as do a BLE scan for devices.(WIP) concurrently 
 or as close as possible.
===========================================================
This example code provides both Push Button method and Pin
based WPS entry to get your ESP connected to your WiFi router.
Hardware Requirements
========================
ESP32 and a Router having WPS functionality
This code is under Public Domain License.
Author:
Pranav Cherukupalli <[email protected]>
*/
#include "WiFi.h"
#include "esp_wps.h"
/*
Change the definition of the WPS mode
from WPS_TYPE_PBC to WPS_TYPE_PIN in
the case that you are using pin type
WPS
*/
#include <BLEDevice.h>
#include <BLEUtils.h>
#include <BLEScan.h>
#include <BLEAdvertisedDevice.h>
#define ESP_WPS_MODE      WPS_TYPE_PBC
#define ESP_MANUFACTURER  "SEEED"
#define ESP_MODEL_NUMBER  "ESP32C3"
#define ESP_MODEL_NAME    "Xiao ESP"
#define ESP_DEVICE_NAME   "ESP STATION"
uint32_t chipId = 0;
static esp_wps_config_t config;
int scanTime = 5; //In seconds
BLEScan* pBLEScan;
class MyAdvertisedDeviceCallbacks: public BLEAdvertisedDeviceCallbacks {
    void onResult(BLEAdvertisedDevice advertisedDevice) {
      Serial.printf("Advertised Device: %s \n", advertisedDevice.toString().c_str());
    }
};
void setup(){
  Serial.begin(115200);
  delay(1000);
  Serial.println();
   for(int i=0; i<17; i=i+8) {
	  chipId |= ((ESP.getEfuseMac() >> (40 - i)) & 0xff) << i;
	}
	Serial.printf("ESP32 Chip model = %s Rev %d\n", ESP.getChipModel(), ESP.getChipRevision());
	Serial.printf("This chip has %d cores\n", ESP.getChipCores());
  Serial.print("Chip ID: "); Serial.println(chipId);
  
	delay(2000);
  WiFi.onEvent(WiFiEvent);
  WiFi.mode(WIFI_MODE_STA);
  Serial.println("Starting WPS"); // GO press WPS button.
  wpsInitConfig();
  wpsStart();
  Serial.println("Scanning...");
 //delay(2000);
  while ( WiFi.status() != WL_CONNECTED) { //Wait for connection
   //Serial.println(WiFi.localIP());
   delay(20000);
   // print the received signal strength:
  long rssi = WiFi.RSSI();
  Serial.print("RSSI:");
  Serial.println(rssi);
  }
}
void loop(){
   //Serial.println(WiFi.localIP ());
 delay (5000);
 //goBlue ();
 
}
void goBlue () {
BLEDevice::init("");
 pBLEScan = BLEDevice::getScan(); //create new scan
 pBLEScan->setAdvertisedDeviceCallbacks(new MyAdvertisedDeviceCallbacks());
 pBLEScan->setActiveScan(true); //active scan uses more power, but get results faster
 pBLEScan->setInterval(100);
 pBLEScan->setWindow(99);  // less or equal setInterval value
 BLEScanResults foundDevices = pBLEScan->start(scanTime, false);
 Serial.print("BLE-Devices found: ");
 Serial.println(foundDevices.getCount());
  Serial.println("BLE-Scan done!");
 pBLEScan->clearResults();   // delete results fromBLEScan buffer to release memory
}
void wpsInitConfig(){
  config.wps_type = ESP_WPS_MODE;
  strcpy(config.factory_info.manufacturer, ESP_MANUFACTURER);
  strcpy(config.factory_info.model_number, ESP_MODEL_NUMBER);
  strcpy(config.factory_info.model_name, ESP_MODEL_NAME);
  strcpy(config.factory_info.device_name, ESP_DEVICE_NAME);
}
void wpsStart(){
    if(esp_wifi_wps_enable(&config)){
    	Serial.println("WPS Enable Failed");
    } else if(esp_wifi_wps_start(0)){
    	Serial.println("WPS Start Failed");
    }
}
void wpsStop(){
    if(esp_wifi_wps_disable()){
    	Serial.println("WPS Disable Failed");
    }
}
String wpspin2string(uint8_t a[]){
  char wps_pin[9];
  for(int i=0;i<8;i++){
    wps_pin[i] = a[i];
  }
  wps_pin[8] = '\0';
  return (String)wps_pin;
}
void WiFiEvent(WiFiEvent_t event, arduino_event_info_t info){
  switch(event){
    case ARDUINO_EVENT_WIFI_STA_START:
      Serial.println("Station Mode Started");
      break;
    case ARDUINO_EVENT_WIFI_STA_GOT_IP:
      Serial.println("Connected to :" + String(WiFi.SSID()));
      Serial.print("Got IP: ");
      Serial.println(WiFi.localIP());
      break;
    case ARDUINO_EVENT_WIFI_STA_DISCONNECTED:
      Serial.println("Disconnected from station, attempting reconnection");
      WiFi.reconnect();
      break;
    case ARDUINO_EVENT_WPS_ER_SUCCESS:
      Serial.println("WPS Successfull, stopping WPS and connecting to: " + String(WiFi.SSID()));
      wpsStop();
      delay(10);
      WiFi.begin();
      break;
    case ARDUINO_EVENT_WPS_ER_FAILED:
      Serial.println("WPS Failed, retrying");
      wpsStop();
      wpsStart();
      break;
    case ARDUINO_EVENT_WPS_ER_TIMEOUT:
      Serial.println("WPS Timedout, retrying");
      wpsStop();
      wpsStart();
      break;
    case ARDUINO_EVENT_WPS_ER_PIN:
      Serial.println("WPS_PIN = " + wpspin2string(info.wps_er_pin.pin_code));
      break;
    default:
      break;
  }
}
Output on Ser.Mon.
ESP32 Chip model = ESP32-C3 Rev 3
This chip has 1 cores
Chip ID: 4196588
Station Mode Started
Starting WPS
Scanning...
RSSI:0
sm BSSid: 00:00:00:00:00:00 scan BSSID d4:04:cd:ff:0e:54
RSSI:-53
Disconnected from station, attempting reconnection
WPS Successfull, stopping WPS and connecting to: GlassSurf-2.4
E (45554) wifi:sta is connecting, return error
RSSI:-54
RSSI:-54
RSSI:-54
RSSI:-54
Disconnected from station, attempting reconnection
Connected to :GlassSurf-2.4
Got IP: 192.168.1.189
RSSI:-54
Works well holds connection NO Issues.
on to BLE’ Scan. (goBlue)
HTH
GL :-p