Hi,
I’m using a LoRa-E5 module to send datas on TTN. The LoRa-E5 is factory programmed, and I use it with AT commands, send by a microcontroller.
I have a TTN gateway, and I achieve to send datas to TTN since some months, without any trouble.
Currently, there are negative temperatures at night, and I don’t receive datas on TTN during nights.
I can reproduce this comportment putting my device in a freezer.
I logged temperatures of the freezer and the temperature returned by the LoRa module. Below -6°C (around 5°C in the module), the LoRa-E5 don’t achieve to send datas.
This is my LoRa-E5 configuration:
AT+LW=VER,103
AT+MODE=LWOTAA
AT+DR=US915
AT+CH=NUM,8-15
AT+JOIN
I send messages with the command AT+CMSGHEX.
TTN answers:
I tried to:
- Activate or not the ADR
- Change the antenna
- Disconnect and connect again the LoRa-E5 to TTN
- Reset the module (software reset and power-cycle)
But there is no change.
When I reset the module, the JOIN fail. When the module go back to ambient temperature, it can communicate.
I also check the power supply, and there is no trouble.
Does anyone use a LoRa-E5 with negative temperature without any trouble?
Is there any other configuration to allow me to communicate with these temperatures?
Thanks,
Anthony