Having Problem with internal memory for XIAO nrf52840 BLE Sense

Good afternoon everyone.

I am am trying to get my XIAO nrf52840 to read/write from the internal memory. Everytime I try to use any kind of LittleFS.h library, it does not recognize the library. I have tried the adafruit version, the arduino version and just using LittleFS.h. I am using Arduino IDE and using the mbed version of the nrf52840 BLE Sense board.

Any insight would be great. I can get the QSPI code on the Seeedstudio main page to work, but looking for a condense simple code.

Thank you.

Hi there,

And Welcome Back, been a while. :v:

So check out the internal external tester code and the tech used to access the Internal and external Flash as well as an additional (added chip) to the grove expansion board bottom.

and this one is just for Fun. :grin:

HTH
Gl :slight_smile: PJ :v:

Looks like the LittleFS libraries aren’t compatible with the mbed core you’re using. I’d stick with the Seeed QSPI examples or look for an mbed-specific filesystem solution.