QSPI Flash Access on Custom XIAO nRF52840 PCB

:crossed_fingers: crossed_fingers: i there,

So , as per usual @msfujino is correct… :grin:

If I may add, have a look at this code and thread on the Grove Expansion Board, It has a spot on the Bottom to Add additional Flash and I have done so. The Testing zcode would be helpful to you.
It tests both the Internal Flash, the External QSPI flash and the Solder-in Flash chip. I did both Nrf52840 & ESP32C3 vastly different configs for the SPI’s

In the END i got it going with Excellent support from The seedineers, @Citric & @Seeed_Seraphina … Check out the complete flash testing Journey and it should be beneficial to you.

HTH
GL :slight_smile: PJ :v:

So in reviewing your open, and Without any code posted I’m betting this link has your answer, it’s subtle…very subtle
You’ll get it just read everything and stay with it. :yum::+1:
also post the code if you can, use the code tags above “</>” and paste it in there. The SPI’s (including the QSPI) are slick and better than how the ESP32 monkeys doit.:grin: IMO.
:crossed_fingers: