I have grove vision ai module. I have trained the keyword detection model using EI and now want to run in real time.
Though, I see that there are some nice examples for object detection using camera, there are not examples that using microphone for keyword detection.
Can you please help?
you need to flash the specialized Edge Impulse audio firmware onto the module and then use the Edge Impulse CLI (Command Line Interface) for real-time inference via a connected computer
There is no direct Arduino example for real-time audio inference using just the Grove AI module itself as the main processor for the audio data.
I found this works…
YMMV:grin:
To run your Edge Impulse keyword detection model in real time on the Grove Vision AI module, you need to use the Edge Impulse CLI (Command Line Interface) tool on your computer, as existing examples focus on the camera. The Grove Vision AI module (original V1) has a built-in microphone, which the Edge Impulse firmware can access for data sampling and inference.
Steps for Real-Time Keyword Detection
Ensure Correct Firmware:
Make sure the Grove Vision AI module is flashed with the latest Edge Impulse firmware. Instructions can be found in the Edge Impulse documentation.
This firmware allows the Edge Impulse CLI to communicate with the board, including accessing its sensors like the microphone.
Connect to Your Computer:
Connect the Grove Vision AI Module to your PC via a USB Type-C cable.
Run Inference using the CLI:
Open a terminal or command prompt on your computer.
Run the following command to start real-time inferencing:
edge-impulse-run-impulse --debug
This command connects to the board, streams the raw microphone data to your computer, runs the trained model, and prints the results to the console in real time.
Observe Results:
The console will display the recognized keywords and their confidence scores as you speak into the microphone.
Alternative: Deployment as an Arduino Library
If you need the module to run autonomously without being connected to a PC via the CLI, you can deploy your model as an Arduino library:
Download the Library: In the Edge Impulse studio, go to the Deployment section and select Arduino library. Download the generated ZIP file.
Install the Library: In the Arduino IDE, go to Sketch > Include Library > Add .ZIP Library and select the downloaded file.
Use the Example Sketch:
Open the example sketch provided within the newly installed library.
The example code often demonstrates how to use the built-in microphone for keyword spotting (look for examples related to Pdm or microphone). You may need to adapt it slightly to fit your specific model’s output and desired actions.
Upload the code to your associated microcontroller (like a Wio Terminal or a XIAO board, as the Grove AI Module typically acts as a coprocessor).
Monitor the serial monitor for the real-time detection results.
Since official examples for the Grove Vision AI module with a microphone are less common compared to camera examples, using the Edge Impulse CLI or the custom Arduino library with its built-in example code are the most reliable methods for real-time operation.
@PJ_Glasso
I know most of the above information and I have followed the docs.
I have trained the model and can do inference using cli.
What I am interested in is using microphone and some code that runs continuously.!
In the library code there were no specific functions related to mic. That is why I asked.
So,
I get a strong inklings from your Questions, you didn’t go through the tutorial or watch the video Then . I won’t spoil it for you , He directly answers your question, Suffice to say " you put the model in “continuous mode”
Funny part is, That one is the easiest and the most full featured models and training tutorials if YOU do the work…
It all Works. Longest part is building the Data sets, the Hello_world, Yes, No. (unknown) and NOISE (everything else).
You can use the MIC on the Board. BTW. or Phone or Xiao PDM.
Easiest I found is to use the Board’s Mic. Mobile phone ,Next and Xiao you load a recorder IMO, record the PDM , 16-bit samples and save them to SD and upload to the EI KWS training model as Set data.
Once it builds, you verify it works , then grab the C compiled BIN or HEX , You load that on your device, Then connect to the serial port of it with computer terminal and Power it up, You can make it boot the code or , kick it off with a terminal command.
I may do a video Walk through with a Xiao, Time permitting. but it is very, very similar in steps and process as the object recognition demo I did a while back on here. Stuff is AWESOME
Here is the Missing LINK in your Evolutionary understanding Watch the WHOLE video!
Run through the How to and LMK were you get stuck.
HTH
GL PJ
Here was a Thread we walked through the Bootloader restoration…:fingers
Interesting project! Running real-time audio models can be tricky without clear examples. Reminds me of how intuitive setups like Y888 make complex tasks feel much easier once you see the workflow in action.
So, Yes the real-time models can be. However the training is the KEY..
Having STRONG “unknown” class as well as “Known” classes are really the grease that makes it go. I have always felt the good ones really know what they “DON"T” want or except vs. what the goal is. LOL .. It’s like " I know it when I see it " or hear it "