Grove Shield for XIAO Questions

Hi there,

a few questions about the Grove Shield for Xiaomi that I couldn’t find the answers to in the wiki.

  1. on the Grove Shield shield i have to solder a lipo like on the seeed. there is no jst2.0 connector like on the Expansion Board Base. Or can i use the Grove connectors for a lipo?

  2. Load Capacity is 800mA. So i cant put a 1000mA or 2000mA lipo on it?

  3. Does it work with a XIAO nrf54l15? The Expansion Board Base doesnt.

Thank you

Hi there,

And welcome here…
SO do you mean this one ?

If so ,Have a look at this one I did…It works GREAT! and you can add a extra flash :+1:

HTH
GL :slight_smile: pJ :v: