I need to use ESP32C3 to communicate with a sensor device through SPI interface. I wonder where I can find SPI sample code for ESP32C3.
Hi there,
in a word, " ALL OVER" ![]()
The C3 mind you isn’t like the others, FYI…
Check out the Demo’s on here, “The Grove Expansion Demo” code has the secret handshake info. ![]()
It’s not rocket Science but a process in instantiating the correct SPI interface and pins.
HTH
GL
PJ
check out the diff’s between Xiao’s for example on Wiki.
To find the SPI code for ESP32C3 in the official ESP-IDF repository.
thx PJ, would you please provide the link?
Hi johnny, would you please provide the link?
Ah’ Check it out We did, You take those keywords or the ones in Quotes and you use the magnifier up in the right corner looks like this.
put that in and BAM! bob’s your uncle… instant info with many sources.
I suppose I could go get the Hard link to the post but I come from the
“Teach a Man to Fish” and he feeds himself and his family club, as opposed to “Give a Man a Fish” and he only eats for today.
Besides I wouldn’t want to deny
Ask any questions you have and post any samples you may have issues with , lots of smart folks on here to help.
HTH
GL
yes, I got your project link.
But the SPI functions details are hidden in
Adafruit_FlashTransport_SPI QflashTransport(PIN_QSPI_CS, SPI_2);
For ESP32C3, what is the first parameter should be for
SPIClass SPI_1(???, D9, D8, D10);
Hi there,
That would be the Chip_Select_pin.
HTH
GL
PJ