Esp32-c6 battery management

Hi, I was just wondering if anyone had some good specs on the battery management used by the esp32-c6. I’m trying to work out if it includes over discharge protection. Also the documentation stats for input BAT is 4.2v. Does anyone know if the board will work with a slightly higher voltage of 4.35v provided by a HV LiPo.

Thanks in advance

According to the schematic, the SGM40567-4.2 is used as the charge controller and can only charge up to 4.2V.
There is no over-discharge protection, so a battery with a protection circuit must be used if necessary.

@msfujino thanks heaps for the quick reply. Appreciate the response. I’ll have to have a better look for the schematic this time.

I measured the charging and got different results:

Charging starts at 4.18 V and ends at 4.20 V charging Voltage. The Voltage will drop slightly below this Level (to 4.18 V) when disconnected after charging. If dis- and reconnected, charging will resume until 4.20 V is reached again.

(ESP32C6 USB on Macbook, Sketch Blink, Li-Ion Battery SLB-11A 1130 mAh)

Next experiment will be, how to calculate Battery status (% of full Battery). For that the measurement of the specific curve of voltage vs. drawn mAh is necessary. It is non-linear. Seeed has an example for measuring the voltage. Look for "seeedstudio, ESP32C6, measuring battery voltage“.

The voltage varies depending on the timing of the measurement. I recommend that you carefully read the following sections of the SGM40567 datasheet.

Figure 4. Charge Profile
Figure 5. Charge Profile
ELECTRICAL CHARACTERISTICS

Maximum Charging Voltage                 4.166   4.20  4.234  V
Output Voltage Fold-Back Holding         95.4    96    96.7   %
Full-Charge Voltage Detection Threshold  97      98.5   -     %

Not ESP32C6, but for your information.

The ESP32-C6 chip does not provide over-discharge protection.
You need to use a dedicated battery protection circuit (many LiPo batteries include one), or a battery management IC like TP4056.

If you need more info about ESP32 low power modes, you can see here:
https://www.theengineeringprojects.com/2021/12/esp32-low-power-modes.html