Electronics Basics ESP32C3 or others

I have a question. I think I’ve figured out the answer, but I know next to nothing about electronics and wanted to check with someone here who surely does. Now, this is an image of a “shield” they call it that I have for a Xiao ESP32C3.

In this image it shows 8 connectors, which have 4 interface types, you have digital–that means the values will be 0 or 1. You have analog which means the values will be a range. You have two that support some sort of protocol UART and I2C.

Please correct me if I got this wrong.

Which brings me to the part I am unsure about, sensors and code.

Now if I have a sensor like a LED, I can plug this into a digital or an analog port? Its a question? Yes, but should a port be solely a I2C or a UART it would make no sense.

Assuming I am on the right track, I need to tell the system not only have I plugged in an LED, but it needs to supply power to it, so in software that looks like this in Arduino speak.

Setup() {
    pinmode(D0,OUTPUT) or maybe pinmode(D0,POWER)?
}

So the basic syntax is the command “pinMode” with the parameters in this case telling it to send power to D0 on the assumption I just want to turn the LED ON or OFF. Would send power to A0 if I wanted to be able to vary the power supplied, to get a brighter or dimmer LED?

Over to management of said LED. Now the piece of code I made up reads the current value of the line D0 and depending on it toggles it to HIGH or LOW with the commands digitalRead and digitalWrite. Commands I assume are linked with the physical control line to the D0 register.

void loop() {
buttonState = digitalRead(D0);
if(buttonState == LOW) {
digitalWrite(D0, HIGH);
}
else {
digitalWrite(D0,LOW);
}

In summary I used different commands on the same register, that in effect map to different bits of hardware

Does all this make sense? Does anybody know of a good book I can get that will help me put the different pieces together like this. In the big scheme of things this isn’t rocket science, if you understand the basics it all makes sense.

Hi there,
So have a look at the “Grove Expansion” :mag: search results of course a Demo I did using it, adding the external Flash chip to the bottom of it Code is included to test it and compiler output versions for the C3 and nRF52840 and 3D printed also some different size cases and holders for it. It is very versatile and easy to use. Displays, One wire Temp probes, switches , bussers, lots of Grove accessories. Allows quick assembly of shakedown prototypes and proof of concepts in both software and Hardware. :v:

The battery management works well and would be even better if they updated it and added a PMIC ic. and that way true battery management can be off MCU board. It’s seeed achilles heal on a lot of there products that purport to be suitable for battery power or wearables. Only the WIO terminal includes a battery management chip you can query a whole host of parameters and even the Battery voltage , Imagine that! SOC,(state of charge) and hrs used for very accurate battery life and management data.
interrupts for certain parameter levels and conditions, I2C configuration makes it a snap…

That is my take on it
HTH
GL :slight_smile: PJ :v:

You’re thinking about it in the right way, and your questions make sense for someone learning electronics. Digital pins are typically used for simple ON/OFF control, while analogue-capable pins can read varying signals or, in some cases output PWM for brightness control, which only simulates analogue output.

For an LED, you’d usually use pinMode(pin, OUTPUT) and then digitalWrite() for ON/OFF. There’s no POWER mode—power is always available through the board’s supply pins, while GPIO pins are for control signals.

Your understanding of digitalRead() it digitalWrite() is solid. The same pin can often be used differently depending on how you configure it in software, which is one of the key ideas in microcontrollers like the ESP32-C3.

A good beginner electronics + microcontroller book can really connect these concepts. Something practical and hands-on will help far more than theory alone. You’re asking exactly the right questions to build that foundation.