DIO and CLK pads on XIAO nRF52840

And same question for the XIAO nRF52840, Is it possible to use the DIO and CLK pads on the back of the XIAO nRF52840 as general purpose GPIO pins ?

Hi there,
I think it’s the same as this one we checked out ? YMMV
Something similar I’ll bet is possible or use the PLUS varriant also?

HTH

GL :santa_claus: PJ :christmas_tree:

But that info is for the ESP32S3, I was asking about the nRF52840.

Different processor, different behavior.

Hi there , yes of course..
It’s the same want is what I was pointing out.

GL :grin::ok_hand:

According to the nRF52840 datasheet,
SWDCLK and SWDIO appear to be debug pins.
They likely cannot be used as GPIO pins.

Huh? How about - “Oops my bad :face_with_hand_over_mouth:”

No, Not a Bad…
Trouble maker. :saluting_face:

WTF , is wrong "it’s something similar …I wanted him to go look and see , but that with the esp32 it IS possible , Is all. Go sell some peanuts or something…

As you were…

Season’s greetings… :christmas_tree:

GL :santa_claus: PJ :v:

If you look closer and stop trying to find Fault always… The MCU name is in the Tittle
There is a “PLUS” in Both mcu family’s .The Bottom Line is THEY BOTH WANT to USE the BOTTOM PADS… or do we need sign language for you. :face_with_peeking_eye:

Hi there,

and Yes, TRUE facts, I was hoping he would go look.
But the peanut gallery was wanting to chime in..So it is as I said.“MAYBE” or Not?

Thank you for the clarification. :+1:

GL :santa_claus: PJ :v: