Hi there ,
Ok so It works no issue’s Led lights every time through the loop the Built-in on io21 and and external connected thru a 220 ohm resistor to 3.3v connected to the bottom pin io42 the Serial output is the touch pin value (typical 24-29) touched over 1000.
Here is the code I used.
const int touch_pin = A5;
int LED_pin = 21;
int MTMS_pin = 42;
void setup(void) {
Serial.begin(9600);
delay (1000);
// declaring LED pin as output
pinMode(LED_pin, OUTPUT);
pinMode(MTMS_pin, OUTPUT);
}
void loop(void) {
// turn on:
digitalWrite(LED_pin, HIGH);
digitalWrite(MTMS_pin, HIGH);
delay(500);
Serial.print("Touch value: ");
Serial.println(analogRead(touch_pin));
delay(1000);
// turn off:
digitalWrite(LED_pin, LOW);
digitalWrite(MTMS_pin,LOW);
delay(500);
}
Here the output;
mode:DIO, clock div:1
load:0x3fce3808,len:0x44c
load:0x403c9700,len:0xbe4
load:0x403cc700,len:0x2a38
entry 0x403c98d4
Touch value: 41
Touch value: 33
Touch value: 18
Touch value: 27
Touch value: 26
Touch value: 1083
Touch value: 1107
Touch value: 1159
Touch value: 25
Touch value: 31
Here is the connected DUT
Got a little HOT when setting the pins, Don’t be in a hurry.
These is the pogo pins.
Bottom Filmed on a Potato So…
Here’s the pins. I connected the White jumper to the MTMS (GPIO42)
MTDI 47 I/O/T VDD3P3_CPU MTDI GPIO41 CLK_OUT1 D12 PDM_DATA GPIO41 MTDI
MTMS 48 I/O/T VDD3P3_CPU MTMS GPIO42 D11 PDM_CLK GPIO42 MTMS
HTH
So you can use the pins on the bottom for IO, AFAIK.
GL
PJ
Here is the ZIP containing the Socket, you can print your own, add the pins and make the legs or look at the other socket thread and see how it’s done. ENJOY.
XiAO_Socket_ESP32S3-Body.rar (59.7 KB)