Android x86 distro / ODYSSEY X86J4105864 / 4G Modem Capability

I used this type of antenna, but any 4G antenna with MHF4 connector can be used.

For checking basic connectivity only one antenna is necessary on MAIN connector, but 4G modem use MIMO (multiple input multiple output) so 2 antennas are required for best performance.
Please note that on 3G modem a second antenna is not strictly necessary but helps to avoid multipath interference signal cancellation.

The 2 antenna must be of the same type.
For GNSS use there are specific antenna with the same MHF4 connector.

Please can you kindly verify if the onboard LANs will be disabled if you put the 4G module on Odissey? I have this big problem without solution for now.
see:

Thanks