Adrucam IMX519 Not working

Hi all,
I have a seed studio j1020 Board with jetson nano which i had extended space using ssd. but from the day of purchase i dont see camera working.

tried with raspberry pi IMX1477 hq camera, 5 mp camera and also adrucam imx519 camera. nothing seems working.

getting below error while trying to install adrucam driver.

Errors were encountered while processing:
arducam-nvidia-l4t-kernel
E: Sub-process /usr/bin/dpkg returned an error code (1)

tried re flashing board using SDk manager but no luck

Below are the board details:
cat /etc/nv_boot_control.conf
TNSPEC 3448-401-0002-G.0-1-0-jetson-nano-devkit-emmc-mmcblk0p1
COMPATIBLE_SPEC 3448-300-0002–1–jetson-nano-devkit-emmc-
TEGRA_CHIPID 0x21
TEGRA_OTA_BOOT_DEVICE /dev/mmcblk0boot0
TEGRA_OTA_GPT_DEVICE /dev/mmcblk0boot1

cat /etc/nv_tegra_release

R32 (release), REVISION: 7.5, GCID: 36557527, BOARD: t210ref, EABI: aarch64, DATE: Tue Jun 11 23:12:44 UTC 2024

1 Like

Hi there,
Interesting to say the least,
You got a picture?
Does either camera work with the RPi?
GL :slight_smile: PJ
:v:

Yes cameras are working in RPI

You can check the answers regarding the error here: Apt upgrade problem: Errors were encountered while processing: nvidia-l4t-bootloader - #3 by JerryChang - Jetson Nano - NVIDIA Developer Forums

Here may explain why the IMX477 HQ camera is not calling properly;

We are very sorry that we have not tried to use the Adrucam IMX519 camera with our boards. Non-NVIDIA official carrier boards do not necessarily support Adrucam’s cameras. We apologize for the inconvenience.