same situation here ….
Spam protection getting in the way … I hope I can now post
Hi there
Yes, I responded to your concern, You should be good to go, or very close by now. ![]()
HTH
GL
PJ ![]()
Going to make a thread regarding spectra 6 and partial updates using the EE04, so need to be able to post topics.
i am replaying here to get new topic button
have you got new topic if u got can u tell me what should i do to get
just to gat “new topic” button … sorry
Hi all, trying to find some information on how the xiao debug mate is supposed to work
Replying so I can post.
Hello xiao category,
I come here to learn about how to post. This is my second reply in what appears to be a three reply threshold before new users can post something new. I searched for my topic but didn’t find it. So, I shall wait several minutes between each of my three replies so I can get the power to start a new thread.
I also just learned that a post has to be at least 20 characters or else it pops up a red message saying that you have to use at least 20 characters. This “About the XIAO category” thread is a treasure trove of information. Apparently there’s also a heart button somewhere. That was the second sentence in the red message. It wanted to know if you had ever used it.
Some posts above say different things about how to get the posting button. They must have changed over time. In my case, I did three replies here, liked a bunch of replies here (about getting the post button, so they were real likes), uploaded a picture, added a bio blurb, snooped around the forum, replied to different post. After that, I got “trust” level. But, no button. I logged out, logged back in. There was the post button. This place feels like a Discourse forum. Everything is gamified. Well, anyway, it took a lot of doing, but I can now post a new thread. I assume. I didn’t try it yet. I had to pop back in here and tell my long story for future travellers. ![]()
I feel like an idiot doing this, but here’s my first reply, so I can post about an actual hardware issue… Sigh.
It’s like being trapped in a Kafka novel. My Seeed Studio account login apparently wasn’t good enough to prove I belong here. Sigh, sigh, sigh…
I think Discourse forum software was made by people who hate forum users. I don’t know why webmasters go with it. Every forum I’ve been on that uses Discourse has a million comments like yours from people who just want to ask a question, not put down roots and raise a family.
I want to post a new thread as well! I have trouble with my new XIAO nRF52840 & Wio-SX1262 Kit, not receiving anything. Newest firmware, no error-output, config is triple-checked and fine. I even bought a shiny new antenna. The kit behaves as there was no antenna connected. So no nodes are found, except the device itself. I am using long fast and EU_868.
Here is my lora-config, as reported by the linux-command meshtastic --port /dev/ttyACM0 --info
"lora": {
"usePreset": true,
"bandwidth": 250,
"spreadFactor": 11,
"codingRate": 5,
"region": "EU_868",
"hopLimit": 3,
"txEnabled": true,
"txPower": 13,
"sx126xRxBoostedGain": true,
"ignoreMqtt": true,
"femLnaMode": "NOT_PRESENT",
"modemPreset": "LONG_FAST",
"frequencyOffset": 0.0,
"channelNum": 0,
"overrideDutyCycle": false,
"overrideFrequency": 0.0,
"paFanDisabled": false,
"ignoreIncoming": [],
"configOkToMqtt": false,
"serialHalOnly": false
Important note: “txPower”: 13 is the correct value for max. antenna-output with lora in germany. The firmware has a wrong (higher!) preset, when choosing EU_868. The wrong preset violates government-restrictions! Firmware is: 2.7.26.54e0d8d. The programmers confused the units dBm and mW (milli-watts).
I use client dot meshtastic dot org to communicate with my device over wifi. In category “nodes” the webseite always shows an SNR of “0 dB 50%”. My device is a SEEED_XIAO_S3. I also can connect with the program gtk-meshtastic-client over serial or show device-output with minicom over the same serial-port /dev/ttyACM0. As you can see: I am using a linux-computer for connections. No strange output so far: My device just doesn’t recieve anything.
ok, I can open topics now too. The key is to read a few threads. The system seems to measure the time of reading.
blah blah blah here’s some spam so that maybe i can post.