About the XIAO category

Seeeduino XIAO - Arduino Microcontroller - SAMD21 Cortex M0+

Seeeduino XIAO is the smallest Arduino compatible board in Seeeduino Family. It is an Arduino microcontroller that is embedded with the SAMD21 microchip. The interfaces of Seeeduino XIAO is rich enough in such a tiny Dev. Board as well.

Key Features

  • Powerful CPU: ARM® Cortex®-M0+ 32bit 48MHz microcontroller(SAMD21G18) with 256KB Flash,32KB SRAM
  • Flexible compatibility: Compatible with Arduino IDE
  • Easy project operation: Breadboard-friendly
  • Small size: As small as a thumb(20x17.5mm) for wearable devices and small projects.
  • Multiple development interfaces: 11 digital/analog pins, 10 PWM Pins, 1 DAC output, 1 SWD Bonding pad interface, 1 I2C interface, 1 UART interface, 1 SPI interface.

Store: https://www.seeedstudio.com/Seeeduino-XIAO-Arduino-Microcontroller-SAMD21-Cortex-M0+-p-4426.html
WiKi: http://wiki.seeedstudio.com/Seeeduino-XIAO/

how can i start a thread on the forum?

I would like to know also

Same here. Didn’t find anything in this regard.

I too have the same issue! Came to the forums with a question, and I can’t start a thread anywhere :frowning:

Assuming it is dependent on real interaction to prove you’re not a bot, I’ve liked a post, and am now posting a reply here hoping it helps!

I must be one of the first people to receive this new 7.5" ePaper Panel too, because I can’t find a single thread mentioning it! Fingers crossed this response gives me the “user level” or whatever I need to post my question in the correct section!

OK can’t find anywhere else to post a question on the XIAO 7.5" ePaper Panel that I have received and trying to setup.

After a couple of days of going around and around in circles of installing - uninstalling all the components I am at a point where I can get text on the screen!!

As far as variables from Home Assistant go I have had mixed results with lockups and Resets required to try another way.

So moved onto using the recommended Puppet Add On in Home Assistant.

Successfully getting the chosen Dashboard shrunk down and ready for the ePaper display.

BUT Every time I try I get this

18:40:53][C][http_request:019]:   Watchdog Timeout: 15000ms
[18:40:54][E][component:188]: Component http_request cleared Error flag
[18:41:13][I][online_image:102]: Updating image http://192.168.1.168:10000/epaper-display/epaper-display?viewport=800x480&eink=2$0
[18:41:23][W][http_request.arduino:116]: HTTP Request failed; URL: http://192.168.1.168:10000/epaper-display/epaper-display?viewport=800x480&eink=2$0; Error: connection refused
[18:41:23][E][component:174]: Component http_request set Error flag: unspecified
[18:41:23][E][online_image:135]: Download failed.
[18:41:24][E][component:188]: Component http_request cleared Error flag
[18:41:30][I][safe_mode:041]: Boot seems successful; resetting boot loop counter
[18:41:30][D][esp32.preferences:114]: Saving 1 preferences to flash...
[18:41:30][D][esp32.preferences:143]: Saving 1 preferences to flash: 0 cached, 1 written, 0 failed
[18:41:43][I][online_image:102]: Updating image http://192.168.1.168:10000/epaper-display/epaper-display?viewport=800x480&eink=2$0
[18:41:53][W][http_request.arduino:116]: HTTP Request failed; URL: http://192.168.1.168:10000/epaper-display/epaper-display?viewport=800x480&eink=2$0; Error: connection refused
[18:41:53][E][component:174]: Component http_request set Error flag: unspecified
[18:41:53][E][online_image:135]: Download failed.
[18:41:54][E][component:188]: Component http_request cleared Error flag

Anyone any ideas on how to get Home Assistant/Puppet/ESPHOME/XIAO 7.5" paper Panel to NOT REFUSE the connection?

So close to this being useful… at the moment it is ePaperweight :slight_smile:

iirc I ditched puppet as the quality was just not up to what we need for this display. Probably great for full resolution, colour displays, but really not ePaper friendly.

I wish I could tell you what I did beyond that. I basically smashed various pieces of the tutorial at it until I got something useful on the screen, then went and read all sorts of other docs for rendering content and drawing lines and such. I ended up with 3 cycling pages that show my air quality levels across the top of all three, and then the lower 9/10ths of the screen cycle through my plant monitors to display their stats/alerts. I’ve got more plant monitors than I can fit in three pages now though, so I’ve got to go back to square one and figure out how to only render the ones with a “problem”.

Made some progress, have got it running with paper and it is looking very good- well as good as 800x480 can deliver :slight_smile:
If I install the yaml using the manual method and have the ePaper display connected by usb everything installs and works.

Using the Wifi Install always fails with an HTTP connection refused.

Also, seeing issues with Puppet that require me to restart it every few hours - still investigating.

I have exactly the same problem. I received the 7.5" ePaper panel, but I have some questions.

Unable to create a post, so replying here to get “trusted” I guess.

I bought the XIAO 7.5" ePaper Panel and have it setup and running nicely with Home Assistant. The one thing I can’t find is how to get the battery status? I’d like to monitor it (preferably in HA) so I know when it needs to be plugged in. I’ve done a bunch of searches, but haven’t found anything yet.

I need technical support, however I cannot open a thread. Hope this will do.

I too need to post a tech support question but don’t see a ‘New Topic’ function anywhere.

I also joined this forum to ask a question, but don’t see any ‘New Topic’ button. I waited 24 hours after joining without success.

How does a new person gain the ability to ask a question?

And so, I discover, after posting my original reply, I immediately get a ‘New Topic’ button.

Thanks!

Well, talk about annoying? You find a forum that may be of help, and there’s no way to post a question.

Did anybody work out how to start a new topic? I’m simply trying to find out how to factory reset a seeedstudio 2CH-EM with AC clamp that I’m using in HA.

I’ve had to create a specific 2.4ghz wifi network for IoT devices, as this one was too far for my standard network.

But, it’s not allowing me to change the SSID/PWD… When I reboot it, it just remembers the old one! I’ve tried the ‘button’, but that’s not doing anything.

I can see I can plug in a USB cable, but not sure what I need to do after that (have tried to SSH to it, but connection refused).

Any help appreciated, on how to fix this, or create a topic in the right area :slight_smile:

Ok, found the fix for those interested. I had to ‘block’ the seeed device with my router, so after a while, it resets back to factory.
I then unblocked it, connected to its local wifi SSID (seeedstudio something)… then connected via web to 192.168.4.1 (its default ip address). It then asks what wifi you want to connect to, and off you go!

replying here to see if I can then start a new topic!

This comment has at least 20 characters.

So, um, what does one have to do to be able to start a new topic here?