Hello –
Several months ago I was able to successfully flash my Orin NX on an A603 to JP 5.1.2 using the steps and files in the wiki.
This week I tried to follow the steps in the wiki (on the same computer, just a fresh download) and flashing fails. On the host side, it times out with “waiting for target to boot up” and the device side serial logs end with:
enable_remote_access
enable remote access
insmod /lib/modules/5.10.120-tegra/kernel/drivers/mtd/mtd.ko
insmod /lib/modules/5.10.120-tegra/kernel/drivers/mtd/devices/qspi_mtd.ko
[ 8.458762] qspi_mtd spi6.0: MX25U51279G (65536 Kbytes)
[ 8.461874] qspi_mtd spi6.0: mtd .name = spi6.0, .size = 0x4000000 (64MiB) .erasesize = 0x00010000 (64KiB) .numeraseregions = 0
[ 8.476432] 1 fixed-partitions partitions found on MTD device spi6.0
[ 8.479900] Creating 1 MTD partitions on "spi6.0":
[ 8.484876] 0x000000000000-0x000004000000 : "Whole_flash0"
insmod /lib/modules/5.10.120-tegra/kernel/drivers/spi/spi-tegra210-qspi.ko
insmod /lib/modules/5.10.120-tegra/kernel/drivers/hwmon/pwm-fan.ko
[ 8.513903] using random self ethernet address
[ 8.514029] using random host ethernet address
[ 8.516718] Mass Storage Function, version: 2009/09/11
[ 8.517339] LUN: removable file: (no medium)
[ 8.522899] LUN: removable file: (no medium)
[ 8.527189] LUN: removable file: (no medium)
[ 8.531671] LUN: removable file: (no medium)
Add /dev/nvme0n1
[ 8.538683] rndis0: HOST MAC ba:61:4d:39:d6:e1
[ 8.541411] rndis0: MAC 52:49:86:57:7b:b1
[ 8.545729] tegra-xudc 3550000.xudc: EP 0 (type: ctrl, dir: out) enabled
bash: cannot set terminal process group (-1): Inappropriate ioctl for device
bash: no job control in this shell
bash-5.0# [ 10.550789] tegra-xusb 3610000.xhci: entering ELPG done
Can you help me figure out what is going on? For what its worth, I’m able to flash to jetpack 6 using the instructions in the wiki but I need jetpack 5.1.2 for my project.