Hi,
Few weeks ago I purchased a Solar Charger Shield V2.2. Could you give
the exacte name of the type of connector used to connect solar pannel
and battery ?
Thank you very much.
Hi there,
here is the cable. https://www.seeedstudio.com/JST-2-Pin-power-connector-p-649.html
Thanks
best rgds
Bill
Thanks
best rgds
Bill
Hello,
Thanks for the info, I have seen this answer and I will buy the cables, but I also need the connector. I have seen both 2.00mm and 2.54mm. I have bought solar charger v2.2 11/19/2014, which one is valid for me? From the wikipedia we can see the type of connector, which one do I choose?
Thanks for the help,
Ricardo
I have seen three different connectors but I can´t decide which one is the proper one:
JST PH 2 pin
JST XH 2 pin
JST XHP-2
Which should I choose? This is info that should come with the solar charger v2.2 shield.
Thanks for the help!
Ricardo
Hi There
this is detail<LINK_TEXT text=“https://seeeddoc.github.io/Open_parts_l … 0050P1.pdf”>https://seeeddoc.github.io/Open_parts_library/res/3410050P1.pdf</LINK_TEXT>