need information about solar charger shield V2.2

Hi,



Few weeks ago I purchased a Solar Charger Shield V2.2. Could you give

the exacte name of the type of connector used to connect solar pannel

and battery ?



Thank you very much.

Hi there,


Hello,



Thanks for the info, I have seen this answer and I will buy the cables, but I also need the connector. I have seen both 2.00mm and 2.54mm. I have bought solar charger v2.2 11/19/2014, which one is valid for me? From the wikipedia we can see the type of connector, which one do I choose?



Thanks for the help,

Ricardo

I have seen three different connectors but I can´t decide which one is the proper one:

JST PH 2 pin

JST XH 2 pin

JST XHP-2



Which should I choose? This is info that should come with the solar charger v2.2 shield.



Thanks for the help!

Ricardo

Hi There

this is detail<LINK_TEXT text=“https://seeeddoc.github.io/Open_parts_l … 0050P1.pdf”>https://seeeddoc.github.io/Open_parts_library/res/3410050P1.pdf</LINK_TEXT> :smiley: