5/20/1011 Update: BenF recently released v3.62.
I really feel that this thread is a joke and will never be productive. Non the less, I will still apply my two cents here.
Most people are complaining about the Menu system (myself included) but that is not the essence here. Making the Quad work properly as an oscilloscope with itās current menu system is job one. You can never please everyone with a Menu system, but you can make the existing product functional; please note that it is not functional in itās present firmware state. It is now only a prototype toy.
If Bure and/or his associates want to limit the Quad to an engineering toy, then he/they should continue to ignore all the improvements that BenF has already made to the DSO Nano. The Quad product prototype phase appears to be over (when the ADC interleave is fixed) and it is time for Bure to respond to user requests that have already been filtered for reasonableness and implemented by BenF. Each and every one of those improvements by BenF has made the Nano a very useful, desirable, and professional tool. It is unfortunate that those with Quads only, can not see the amazing results of the DSO Nano firmware improvements in BenFs v3.61 release.
Bottom line, Bure and/or associates; it is time to stop thinking prototype toy and instead switch to usability. You were fortunate that BenF covered for you and fixed the DSO Nano for you while you were elsewhere engineering the Quad, but that will most likely not happen on this go-around for several reasons, not the least being the non-release of the FPGA source code.
Just to clear the air on this topic, listed below is BenFās latest Revisions.txt file which clearly shows what features are desired by the Forum users. This is a clear road map of what issues need to be addressed first (yes, a few items are not related, but most are) and if you would just incorporate these fixes, then your prototype toy would turn into a viable, useful and professional tool. It helps to read this list from bottom to the top.
For those who donāt know what some of these changes mean (Bure and/or associates included) just download BenFās V3.61 update and read the enclosed Userās Guide (isnāt that novel, a Userās Guide to explain the update features). It is time for Bure and/or his associates to either put out or sub-contract these types of changes or the Quad will surely die as an unusable tool.
BenF APP V3.61 - 2011.02.26
- Invert duty cycle when using falling edge trigger
- Add separate controls for buffer priority mode and fast/normal sampling speed
- Adjust trigger position subject to buffer priority
- Fix issue with FIT when in fast sampling mode
- Add option to reset to factory defaults
- Updated firmware users guide
BenF APP V3.60 - 2011.02.17
- Support loading of XML files for primary and reference channel
- Set DSO parameters on XML import (from XML profile section)
- Add sampling rate to XML profile section
- Support reference waveform resizing
- Reference waveform increased from 300 points to 1024 points
- Remove support for DAT reference files (replaced with XML)
- Add fast sampling mode (10 times faster than standard mode)
- Force fast sampling when in real-time scan mode
- Add high/low pulse width measurement
- Modified behavior and appearance of buffer position marker
- Updated firmware users guide
BenF APP V3.52 - 2011.02.04
- Tune precision to accuracy (reduce measurement fluctuations)
- Change to use 6 range gain calibration (recalibration required)
- Improved arithmetic precision across V/Divās
- Improved gain coherence across T/Divās
- Improved accuracy for Gnd Pos calibration
- Display gain calibration as % of full range
- Make saved reference waveform the active reference
- Adjust GndPos in steps of 5
- Display Gnd Pos level (-95 to +95)
- Updated firmware users guide
BenF LIB V3.52 - 2011.02.03
- Set power-on vertical bias offset to 50%
- Adjust ADC prescaler
BenF APP V3.51 - 2011.01.25
- Automatic ground level calibration
- Allow off screen trigger level
- Pressing B for Gnd Pos will reset position to vertical center
- Updated firmware users guide
BenF APP V3.50 - 2011.01.20
- Support waveform resizing (zoom in/out)
- Add vertical scroll capability
- Add under/over voltage indicator (V/Div turns red)
- Fix issues with static display of waveforms when in SCAN mode
- Increased numeric precision (XML val, Vpp, Vmin, Vmax, Vavg)
- Updated firmware users guide
BenF APP V3.43 - 2011.01.09
- Fix issue with inaccurate sample time interval for 2s/Div and 10s/Div
- Adjusted logic for trigger icon coloring (always go red when trigger absent)
- Updated firmware users guide
BenF APP V3.42 - 2011.01.02
- Support SD card hot swap
- Updated firmware users guide
BenF LIB V3.42 - 2011.01.02
- Trigger external interrupt when SD card inserted
BenF APP V3.41 - 2010.12.23
- Support loading (profile, waveform) from arbitrary named files
- Allow sensitivity lines to remain visible when adjusting trigger level
- Cancel FIT mode (change to AUTO) when manually adjusting V/Div, T/Div or trigger level
- Updated ReadMe
BenF APP V3.40 - 2010.12.16
- Increased max sampling rate from 857ks/s to 1Ms/s
- Add measurement for pulse count (count of low-to-high transitions)
- Reconfigure PA1 to analog-in if connected to PA0 (digital pullup conflict with PA0/Ain for V2 owners)
- Adjusted levels for battery state (full >= 3.50, 3.50 > half >= 3.33, 3.33 > low >= 3.16 , empty < 3.16)
- Calculate measurements in scan mode
- Add support for XML export when in scan mode
- Adjusted AUTO mode trigger timer (exclude pre-fetch time)
- Adjusted red trigger icon coloring (when scanning for trigger only)
- Reuse LIB stack memory segment in APP
- Increased sampling depth from 3072 to 4098
- Adjusted FIT mode T/Div sensititivity (prevent osscillation)
- Updated ReadMe
BenF LIB V3.40 - 2010.12.11
- Changed icons for edge triggers and delta
BenF APP V3.33 - 2010.12.11
- Fix issue with calibrated gain not being restored after a power cycle
BenF APP V3.32 - 2010.12.01
- Fix issue with gain not settable for some ranges
- Fix issue with time cursor offset error
- Swap left/right keys for T/Div and V/Div (change to waveform centric)
- Adjust duty cycle subject to HW V1/V2 differences
- Display detected HW version (V1 or V2) on startup screen
BenF APP V3.31 - 2010.11.30
- Fix issue with unable to select 1MHz output frequency
- Fix issue with AUTO trigger in post priority mode
BenF APP V3.30 - 2010.11.28
- Use interpolated waveform drawing for narrow T/divās (less equal 20us)
- Documentation on FILExxx.DAT reference export/import format added to readme
- Tuned FIT mode for faster response and more accurate scale selections
- Made AC measurements (Vrms and Duty) calculations relative to Vavg
- Trigger position preserved across V/Div and T/div changes
- Support screen capture with measurements (select ME and press B or long M)
- Support fine tuning of output frequency (3-digits, range 10Hz-1MHz)
- Option to specify duty-cycle (PWM) for output frequency in 1% increments from fully-on to fully-off
- Added support for full calibration (separate offset and gain for all ranges)
- Added option to set sampling buffer usage priority (pre/post equal split or post priority)
- Changed LIB/APP interface to use runtime function pointer resolve through interrupt vector
- Changed to new extended profile format
- Updated ReadMe
BenF LIB V3.30 - 2010.11.28
- Changed LIB/APP interface to use runtime function pointer resolve through interrupt vector
- Added APP detect with version control
BenF APP V3.21 - 2010.11.23
- Fix issue with incorrect display of trigger position when T/div less equal 20us
- Fix issue with incorrect āWrite Errā message when saving profile and reference files
BenF APP V3.20 - 2010.11.21
- Added support for SD directory and file creation (FAT16 and FAT32)
- Removed template files from distribution (no longer needed)
- Snapshots of the full DSO sampling buffer can be exported to XML files
- Per category file limit extended from 255 to 999
- File sequence numbers default to the highest number used plus one within each category
- File load functions will limit choice of names to existing files only
- File save functions will display existing file names with the color red
- A progress indicator is displayed when saving bitmap images and Xml files
- Option to configure grid light intensity (8 levels) added to menu group OT
- Added low end 0.2V scale for 10x attenuation probes
- Loss of trigger will show as red colored trigger indicator (top left rising/falling symbol)
- Updated ReadMe
BenF LIB V3.02 - 2010.11.21
- Add a verification/retry step to SD card initialization
BenF APP V3.12 - 2010.11.15
- Fix issue with incorrect range calibration
BenF APP V3.11 - 2010.11.08
- Fix issue with calibrate range displaying 0.x% for 10.x%
BenF APP V3.10 - 2010.11.08
- Improved SD card compatibility
- Support two point basic unit calibration
- FI menu group will now default to Save Img
- Readme and revision file added to distribution
- Added template files to distribution