I am still working on this and nearing completion. Basic animations are: Sunny, Cloudy, Raining, Thunderstorm, and Fog. The thunderstorm animation will also make small tornado in the chamber! 
Debugged:
* Wifi Connect
-
Wunderground Weather Parse -
Temp -> LED Color -
Lightning Effects -
Fan Control -
Wifi AP for initial wireless config (using smartphone) -
Set weather location and UTC offset during config -
Time sensitive forecast (today's forecast is in the past at night)
Issues:
-
wio link resets after a dozen minutes or so, WD timeout? -
Wifi Credentials are sometimes forgotten through power cycle, may need to re-write the save process to use the eeprom
Todo:
-
Hardware: Atomizer. Tested ok on breadboard -
Hardware: Water Pump, have the parts -
Hardware: Configuration / Mode select button, the built in config button on D0 seems to be tied into the reset circuit if held too long. -
Software: Elevated forecast, reads tonight and tomorrow, displays worse of the two -
Software: Demo Mode (cycle through temperture colors while cycling through clouds / lightning / vortex) -
Software: Party Mode (Fog with sound reactive lightning, black alt color)