Stalker P5/P6 and Base Shield

Can I move P5 and P6 to go through my base shield? After studying the schematics, I get that you created a conflict with the uarts and the bee, now the question is; how can I have both. I want to upload and debug with the serial monitor -AND- have the xbee running. As far as I know, cannot do that without moving p5 and p6 to remove the conflict?

Can I move p5 and p6 two digital inputs on a base shield; P5-D5, P6-D6?

Do I melt the connector on the topside of the board and then solder two wires up to the shield D5 and D6?

~David