Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

info about ReSpeaker series products

Moderators: lily.li, salmanfarisvp, violet, seth.welday

Post Reply
ningma97
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Thu Sep 06, 2018 8:07 pm

Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

Post by ningma97 » Thu Sep 27, 2018 8:03 pm

Hi,

I've been using the Mic Array v2.0 via the micro USB with a Pi but is it possible to connect it via the pins at the base?

Any advice appreciated.

Ning

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

Post by bill.yu » Fri Sep 28, 2018 3:33 pm

HI Ning

Yes, you can. please follow below connection. thanks.

Image

Image

cheers
Bill

ningma97
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Thu Sep 06, 2018 8:07 pm

Re: Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

Post by ningma97 » Mon Oct 01, 2018 11:05 pm

Thanks Bill.

I can see from the picture that you connected the 2 USB pins, the VDD_5V and the AUX_SEL.

Would it be possible to control the central LED and the LED ring with this connection?

Also please advice which USB pins I should connect. Is the following correct?

USB <--> MicArray
VDC <--> VDD_5V
D+ <--> USBDP
D- <--> USBDM
GND <--> AUX_SEL

Best
Ning

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

Post by bill.yu » Tue Oct 16, 2018 4:00 pm

Hi Ning,

Please follow below connection and you can control the leds as well. thanks.

USB <--> MicArray

VDC <--> VDD_5V
D+ <--> USBDP
D- <--> USBDM
GND <--> GND

ningma97
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Thu Sep 06, 2018 8:07 pm

Re: Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

Post by ningma97 » Mon Oct 29, 2018 6:24 pm

Thanks. So to double check the USB Ground Pin needs to connect to one of the ground pins on the board?

The picture you sent suggests the USB Gnd connects to AUX_SEL.

Also would the board still work if I remove the Audio Jack? It's really in my way and I don't need it. An audio jack on the other side of the board would be much better.

Many thanks.
Ning

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Is it possible to connect Mic Array v2.0 to a Raspberry Pi via the pins at the bottom?

Post by bill.yu » Tue Oct 30, 2018 11:41 am

Hi Ning

It shall be GND, it is my bad. thanks.

USB <--> MicArray
VDC <--> VDD_5V
D+ <--> USBDP
D- <--> USBDM
GND <--> GND

Post Reply