Wio GPS Board- Building up a Simple HTTP Client Connection

Simplify IoT Development.

Moderators: lily.li, violet, seth.welday

Post Reply
markus.schmeckenbecher
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Sat Jan 11, 2020 2:44 am

Wio GPS Board- Building up a Simple HTTP Client Connection

Post by markus.schmeckenbecher » Sat Jan 11, 2020 5:40 pm

Dear ALL,
I use the following example from Seeed to built up a GPRS connection. I wanted to add to that code a Arduino HTTP Client.
The definition of the WIFI client is as follows:

WiFiClient wifi;
HttpClient client = HttpClient(wifi, serverAddress, port);


Based on the Fact that I have only GSM and not WIFI on Board, how should the HTTP definition look like to do the coding?
On the Header I can see the declaration

GPRS gprs = GPRS().

If I put in the HPPT Client (gprs, serverAddress, port), but it doesn't work.
Any Ideas?

User avatar
salmanfarisvp
Elementary-1
Elementary-1
Posts: 177
Joined: Sun May 20, 2018 2:02 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: Linklt One , BeagleBone Green , ReSpaker
Contact:

Re: Wio GPS Board- Building up a Simple HTTP Client Connection

Post by salmanfarisvp » Sun Jan 12, 2020 12:38 pm

Hi,

Which board you are using?
Thank You :) .


Post Reply