TLS support Wio LTE Cat M1/NB-IoT Tracker

Simplify IoT Development.

Moderators: lily.li, violet, seth.welday

Post Reply
guy.dillen159
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Sun Jun 02, 2019 1:42 am

TLS support Wio LTE Cat M1/NB-IoT Tracker

Post by guy.dillen159 » Fri Jun 07, 2019 7:30 pm

Hello,

Here http://wiki.seeedstudio.com/Wio_LTE_Cat ... T_Tracker/ is mentioned this is supported: "Embed protocol: TCP/UDP/FTP/HTTP/HTTPS/FTPS/TLS/MQTT/CoAP". Where can I find info of how to use TLS (https and/or mqtt-s) with the Wio LTE Cat M1/NB-IoT Tracker?

Thanks.
Guy

jeflux
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Sep 02, 2019 5:44 am

Re: TLS support Wio LTE Cat M1/NB-IoT Tracker

Post by jeflux » Mon Sep 02, 2019 9:14 am

Regarding mqtt-s: I was looking to use secure MQTT (AWS Iot). This appears to NOT have initially been supported in the firmware for the ublox cell module included, but supposedly is possible with a firmware update to the SARA-410M-02B module.

I was having other issues while trying to read subscribed message topics via MQTT also.

The latest firmware was released on May 20, 2019 and is version L0.0.00.00.05.08

Unfortunately, I am still trying to figure out how to update firmware. ublox forum members indicate that ublox support has to provide the files and tool directly, so I have an open request at moment. Fingers crossed.

I'm hoping the firmware update will address the issues I'm having.

bill.yu
Junior-7
Junior-7
Posts: 733
Joined: Mon Apr 02, 2018 11:05 am

Re: TLS support Wio LTE Cat M1/NB-IoT Tracker

Post by bill.yu » Thu Sep 19, 2019 3:07 pm

Hi there~

You can burn the SARA-R410M firmware through the RST/DIO/CLK/GND/3.3v @ backside of the D38 port. thanks.

Image

Post Reply