Raspberry Pi 3 B+ & 4 mic array

Applications/questions using Raspberry Pi with Seeed products, please post it here.

Moderators: lily.li, salmanfarisvp, violet

Post Reply
nlukeking
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Aug 16, 2018 4:35 pm

Raspberry Pi 3 B+ & 4 mic array

Post by nlukeking » Thu Aug 16, 2018 5:10 pm

Hello everyone.

I'd appreciate any help in trying to use the 4 mic array hat for raspberry pi 3 b+. It works just beautifully (thank you) on board as the hat.

However, when I take it off board (not just pushed into all of the pins as I am going to need many of the pins for sensors and IR and RF.

I've used the pinout diagram on page 3 of the attached official doc. It's not working. Is this incorrect? If so, what are the essential pinouts to make it function. It would seem that it certainly doesn't need all of the GND or 5VO.

Any help would be greatly appreciated as the forum contains nothing, nor does there seem to be any documentation. Perhaps something that SEEED could provide to it's users?

Thanks.

Nathan
Attachments
ReSpeaker 4-Mic Array for Raspberry Pi - Features.png
ReSpeaker 4-Mic Array for Raspberry Pi - Features.png (755 KiB) Viewed 2092 times

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Raspberry Pi 3 B+ & 4 mic array

Post by bill.yu » Fri Aug 17, 2018 12:04 pm

Hi there,

We have 2 Grove ports on board, one is GPIO(GPIO12 and GPIO13), the other is I2C SDA and SCL. For the sensors, what's kinds of protocol do they use?
If both of them are using GPIO, we can use separate GPIO grove port to 2 Grove ports to connect with 2 GPIO sensors. thanks.

Bill

nlukeking
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Aug 16, 2018 4:35 pm

Re: Raspberry Pi 3 B+ & 4 mic array

Post by nlukeking » Mon Aug 20, 2018 2:59 pm

Hi Bill

I'm assuming your reply was meant for another thread? It doesn't seem to be related.

Nathan

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Raspberry Pi 3 B+ & 4 mic array

Post by bill.yu » Mon Aug 20, 2018 3:35 pm

Hi Nathan,

What's the detail issue do you meet on the schematic? thanks.

Image

Bill

nlukeking
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Aug 16, 2018 4:35 pm

Re: Raspberry Pi 3 B+ & 4 mic array

Post by nlukeking » Mon Sep 10, 2018 12:43 pm

hi @bill.yu

My questions are in my original post.
However, when I take it off board (not just pushed into all of the pins as I am going to need many of the pins for sensors and IR and RF.

I've used the pinout diagram on page 3 of the attached official doc. It's not working. Is this incorrect? If so, what are the essential pinouts to make it function. It would seem that it certainly doesn't need all of the GND or 5VO.
I'm especially interested in the GND and power as I'd like to use them to add additional things to the Pi.

Thanks.

Post Reply