I live in South Africa. I bought two ReSpeaker 2-Mike Pi HAT cards yesterday, to use as the audio interface on Raspberry PI Zero W. I want to build a Google Assistant using this setup. I am using your procedure to install the driver, but it is not working. I am using Raspbian Stretch released in November 2018.
I have not installed any power to the ReSpeaker board, but I am wondering if this is causing the problem - should I connect power to the ReSpeaker board as well?.
Can I use the latest Buster image instead?
Regards,
Brian.
Hi Brian~
- We built a image with driver and avs installed. You can download 2018-08-06-raspbian-for-respeaker.zip
image and burn to sd card. Then plug sd card to raspberry pi directly. You can use thearecord -l to detect the pi hat.
<LINK_TEXT text=“https://v2.fangcloud.com/share/7395fd13 … 13&lang=en”>https://v2.fangcloud.com/share/7395fd138a1cab496fd4792fe5?folder_id=188000207913&lang=en</LINK_TEXT>
- We just tested it and it is compatible. thanks.
</s>pi@raspberrypi:~ $ arecord -l
**** List of CAPTURE Hardware Devices ****
card 1: seeed2micvoicec [seeed-2mic-voicecard], device 0: bcm2835-i2s-wm8960-hifi wm8960-hifi-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
pi@raspberrypi:~ $ uname -a
Linux raspberrypi 4.19.50-v7+ #896 SMP Thu Jun 20 16:11:44 BST 2019 armv7l GNU/Linux<e>
Thank you for your trouble.
Regards,
Brian.