Test Bluetooth Bee on a Mac

wireless communication and related Bees.

Moderators: lily.li, violet, jessie

Post Reply
User avatar
ilcl4z
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sat Sep 25, 2010 5:23 pm

Test Bluetooth Bee on a Mac

Post by ilcl4z » Sat Sep 25, 2010 5:41 pm

Hi!
I bought a Seeeduino Stalker and a Bluetooth Bee and I'm testing these "little toys for big boys" ;-) To program Seeeduino I bought an UartSBee V3.1 too.

Now I wanna test the bluetooth via Terminal on my Mac to try some bluetooth module commands, but I can't do that.
Using "screen /dev/tty.usbserial-A100eFmp 38400" I can connect to the module but I receive "ERROR" from everything I text next.

If I reset the module while I'm connected, I receive
WORK:MASTER

+BTSTATE:0

+BTSTATE:1
but next, only ERROR

Can you help me?

Another question: can I connect uart to seeeduino with bt bee on top? Can I use both together?

Thanks to everyone!
Alessandro

Icing
Elementary-1
Elementary-1
Posts: 140
Joined: Wed Oct 21, 2009 10:39 pm

Re: Test Bluetooth Bee on a Mac

Post by Icing » Tue Sep 28, 2010 8:56 pm

Hi,

You can get more on how to use Bluetooth Bee by searching in the forum.
Here is the link:
http://www.seeedstudio.com/forum/viewto ... uetoothBee

The critical part is to ensure you have sent the right command to the module and it is
successfully received.

Another question:
The module must be unplugged from the stallker when you program to the stallker, as they
are using the same hardware serial port.


May this helpful to you, and please free to ask any question.

All the best,

-Icing

User avatar
ilcl4z
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sat Sep 25, 2010 5:23 pm

Re: Test Bluetooth Bee on a Mac

Post by ilcl4z » Thu Sep 30, 2010 7:11 pm

I read all these stuff but I working on a Mac so I can't use sscom32.exe

After a lot of searching, I found a simple serial port terminal application that allow me to "test" BTbee "by hand".
This tool is CoolTerm (http://freeware.the-meiers.org/).

I attached to this post my configuration.
With this, every command I wanna send to the bt module is something like this
(return)+INQ=0(return)
CoolTerm sends CR+LF every time I press the return button on my keyboard and "local echo" allow me to track every command I send to the module. It's very simple working like this. On a Mac.

Thanks for all!
Attachments
Schermata 2010-09-30 a 13.01.19.png
Schermata 2010-09-30 a 13.01.19.png (72.87 KiB) Viewed 6982 times

Icing
Elementary-1
Elementary-1
Posts: 140
Joined: Wed Oct 21, 2009 10:39 pm

Re: Test Bluetooth Bee on a Mac

Post by Icing » Fri Oct 01, 2010 2:28 pm

Hi Alessandro,

Have you made it success?

Try to use CR option instead of CR+LF.

Regards,

-Icing

User avatar
ilcl4z
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sat Sep 25, 2010 5:23 pm

Re: Test Bluetooth Bee on a Mac

Post by ilcl4z » Fri Oct 01, 2010 2:43 pm

Icing wrote:Have you made it success?
Yes! With this configuration I can manage the BT module from my Mac.
CR+LF is correct.

The situation is that
Mac > USB cord > UartSBee (with switch on position 3v3) > BTBee

with CoolTerm configured like in the previous post.

neufuture
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Tue Oct 12, 2010 5:12 am

Re: Test Bluetooth Bee on a Mac

Post by neufuture » Tue Oct 12, 2010 5:16 am

Hey Alessandro,
I'm trying to setup this as well on Mac with coolterm. I cannot get the bluetooth to be discoverable by my mac. Did you set it up as a slave? If so can you let me know what commands you gave it???

User avatar
ilcl4z
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sat Sep 25, 2010 5:23 pm

Re: Test Bluetooth Bee on a Mac

Post by ilcl4z » Tue Oct 12, 2010 2:23 pm

neufuture wrote:Hey Alessandro,
I'm trying to setup this as well on Mac with coolterm. I cannot get the bluetooth to be discoverable by my mac. Did you set it up as a slave? If so can you let me know what commands you gave it???
To be discovered, first you have to set the bt bee as SLAVE, with command \r\n+STWMOD:0\r\n, and next allow it to be visible, with command \r\n+INQ=1\r\n

neufuture
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Tue Oct 12, 2010 5:12 am

Re: Test Bluetooth Bee on a Mac

Post by neufuture » Tue Oct 12, 2010 2:52 pm

great think i got it working. Do you have to set inquiry every time you start?

User avatar
ilcl4z
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sat Sep 25, 2010 5:23 pm

Re: Test Bluetooth Bee on a Mac

Post by ilcl4z » Tue Oct 12, 2010 3:30 pm

neufuture wrote:great think i got it working. Do you have to set inquiry every time you start?
Yes, at every start

Icing
Elementary-1
Elementary-1
Posts: 140
Joined: Wed Oct 21, 2009 10:39 pm

Re: Test Bluetooth Bee on a Mac

Post by Icing » Tue Oct 12, 2010 8:49 pm

Hi there,

You just need sending command "\r\n+STAUTO=1\r\n" one time,
then Bluetooth Bee will be auto-connected with your PC without setting "\r\n+INQ=1" every time it starts up.

Cheer,

-Icing

Post Reply